Skip to main content
Associate II
April 7, 2025
Question

Eliminating Swap Region to reduce boot time (STM32H753ZI)

Hi Team,

I am new to SBSFU, and our team requires two image examples. To reduce boot time, I need to eliminate the complete swap region, and I am currently working on this.

  1. I will flash the SBSFU binary, including only the SBSFU application, using the user button to update the firmware from a local download.
  2. After the download, I will decrypt the data and attempt to start the application from the download slot.

Could you please suggest the best approach to eliminate the swap region?

Regards,
Rahul

This topic has been closed for replies.

1 reply

ST Technical Moderator
April 28, 2025

Hello @rahulz916 

If my understanding is correct, you ask for SBSFU with single image where no swap area is allocated. 

If it is the case, refer to UM2262 "Appendix C Single-slot configuration" and to the project provided in the SBSFU package with single image for STM32H753 (~\SBSFU_Legacy\STM32CubeExpansion_SBSFU_V2.6.2\Projects\NUCLEO-H753ZI\Applications\1_Image)

 

Best Regards