Skip to main content
Mikhail Soloviev
Visitor II
Oct 19, 2018 12:14 PM UTC
Question

Dual-image FW upgrade using serial stand-alone flash

Hi everybody,

I wonder if it is possible to configure the X-CUBE-SBSFU expansion to use external serial flash chip instead of internal memory. Any ideas, application note?

regards

Mikhail

This topic has been closed for replies.

1 reply

ADach
Visitor II
Apr 2, 2019 11:48 AM UTC

Hi,

I'm actually working on the same topic. Actually, this is possible to download the new firmware image in external flash memory but you have to keep slot 0 in internal flash to be able to execute it.

Regards