Skip to main content
MGowd.11
Associate
February 7, 2020
Question

Does X-CUBE-SBSFU support the external flash on the SPI ?

  • February 7, 2020
  • 5 replies
  • 1582 views

Does X-CUBE-SBSFU support the external flash on the SPI for the secure boot and secure firmware updates ? If yes could you please provide more details if there is any reference boards which has this support. 

Thanks in Advance,

Best Regards,

Gowda

This topic has been closed for replies.

5 replies

Jocelyn RICARD
ST Employee
February 7, 2020

Hello Gowda,

in the latest release of SBSFU (2.3.0) you have an example addressing external OctoSPI flash trough On The Fly decoder.

this is the project:

STM32CubeExpansion_SBSFU_V2.3.0\Projects\STM32H7B3I-DK\Applications\2_Images_ExtFlash

Best regards

Jocelyn

MGowd.11
MGowd.11Author
Associate
February 12, 2020

Hello Jocelyn,

Thanks for the reply, by mistake I missed to use "reply" while writing to you, I am writing my question again.

Is there any example reference with the normal SPI mode supporting the external flash on STM32L496 in SBSFU 2.3.0?

If not, is it straightforward to integrate the existing external flash memory drivers on STM32L496 application to the bootloader SBSFU ? are there any risks in adapting to secure boot environment ? If would be helpful if you can throgh some light on this feasiblity and necessary steps to be taken care. Thanks!

Best Regards,

Gowda

MGowd.11
MGowd.11Author
Associate
February 10, 2020

​Hello Jocelyn,

Thanks for the reply.

Is there any example reference with the normal SPI mode supporting the external flash on STM32L496 in SBSFU 2.3.0?

If not, is it straightforward to integrate the existing external flash memory drivers on STM32L496 application to the bootloader SBSFU ? are there any risks in adapting to secure boot environment ? If would be helpful if you can throgh some light on this feasiblity and necessary steps to be taken care. Thanks!

Best Regards,

Gowda

Jocelyn RICARD
ST Employee
February 13, 2020

Hello Gowda,

There is no such example SPI mode in SBSFU.

The issue is that firmware code will be in clear in the external flash. We cannot promote such setup.

Now, if you still want to go this way, you have QSPI example in the STM32L4 Cube FW.

STM32Cube_FW_L4_V1.15.0\Projects\32L496GDISCOVERY\Examples\QSPI\

And for integration with SBSFU you can take the STM32H7B3I-DK as example, removing the management of the key used for On The Fly Decoding.

Best regards

Jocelyn

MGowd.11
MGowd.11Author
Associate
February 17, 2020

Hello Jocelyn,

Thanks for the reply and your suggestions, We will look into the references mentioned. Thanks!

Best Regards,

Gowda