Skip to main content
Associate III
Feb 26, 2025 10:28 PM UTC
Solved

Debug Authentication Failed

My H5 DK board is in TZ-CLOSED state (after --sfi-flash), I am unable to put it in "Level 1/2/3 Intrusive Debug" state no matter what combinations of keys and certificates to use (including key_1_root.pem and cert_root.b64). Only Full regression works. Any suggestions?  Thanks!

 

17:16:50 : Start Debug Authentication Sequence
17:16:50 : SDMOpen : 602 : open : SDM API v1.0
17:16:50 : SDMOpen : 603 : open : SDM Library version v1.1.0
17:16:50 : open_comms : 495 : open : Asserting target reset
17:16:50 : open_comms : 499 : open : Writing magic number
17:16:50 : open_comms : 509 : open : De-asserting target reset
17:16:50 : open_comms : 561 : open : Communication with the target established successfully
17:16:50 : discovery: target ID.......................:0x484
17:16:50 : discovery: SoC ID..........................:0x00000000_35353537_3332510A_003A002B
17:16:50 : discovery: SDA version.....................:2.4.0
17:16:50 : discovery: Vendor ID.......................:STMicroelectronics
17:16:50 : discovery: PSA lifecycle...................:ST_LIFECYCLE_TZ_CLOSED
17:16:50 : discovery: PSA auth version................:1.0
17:16:50 : discovery: ST HDPL1 status.................:0x2717
17:16:50 : discovery: ST HDPL2 status.................:0x400003bf
17:16:50 : discovery: ST HDPL3 status.................:0xffffffff
17:16:50 : discovery: Token Formats...................:0x200
17:16:50 : discovery: Certificate Formats.............:0x201
17:16:50 : discovery: cryptosystems...................:Ecdsa-P256 SHA256
17:16:50 : discovery: ST provisioning integrity status:0xeaeaeaea
17:16:50 : discovery: permission if authorized...........:Full Regression
17:16:50 : discovery: permission if authorized...........:To TZ Regression
17:16:50 : discovery: permission if authorized...........:Level 3 Intrusive Debug
17:16:50 : discovery: permission if authorized...........:Level 2 Intrusive Debug
17:16:50 : discovery: permission if authorized...........:Level 1 Intrusive Debug
17:16:50 : discovery: permission if authorized...........:Level 3 Intrusive Non Secure Debug
17:16:50 : discovery: permission if authorized...........:Level 2 Intrusive Non Secure Debug
17:16:50 : discovery: permission if authorized...........:Level 1 Intrusive Non Secure Debug
17:17:22 : Start Debug Authentication Sequence
17:17:22 : SDMOpen : 602 : open : SDM API v1.0
17:17:22 : SDMOpen : 603 : open : SDM Library version v1.1.0
17:17:22 : open_comms : 495 : open : Asserting target reset
17:17:22 : open_comms : 499 : open : Writing magic number
17:17:22 : open_comms : 509 : open : De-asserting target reset
17:17:22 : open_comms : 561 : open : Communication with the target established successfully
17:17:22 : [00%] discovery command
17:17:22 : [10%] sending discovery command
17:17:22 : [20%] receiving discovery
17:17:22 : [40%] loading credentials
17:17:22 : [50%] sending challenge request
17:17:22 : [60%] receiving challenge
17:17:22 : [70%] signing token
17:17:22 : SDMAuthenticate : 1317 : client : Found 1 certificates
17:17:22 : [80%] sending response
17:17:22 : [90%] receiving status
17:17:22 : Error: Debug Authentication Failed

This topic has been closed for replies.
JohnyKessler
JohnyKesslerBest answer
ST Employee
Feb 27, 2025 3:38 PM UTC

Hello @Thatseasy 

If I'm not mistaken, you are working with the Secure Manager. In this context, the DA's permissions do not allow reopening the debug for the secure domain. Even if you change the DA's permissions, they will not be taken into account.

You may observe in your traces "discovery: permission if authorized" -> It depends on the configuration.

In TZ-Closed, there is no need to reopen the debug for the nonsecure domain because it is allowed natively.

 

For more information about the product state in the Secure Manager context, please refer to this UM: https://www.st.com/resource/en/user_manual/um3254-secure-manager-for-stm32h573xx-microcontrollers-stmicroelectronics.pdf -> Chapter 6.3 Product state

 

Best regards

Johny

2 replies

JohnyKessler
JohnyKesslerBest answer
ST Employee
Feb 27, 2025 3:38 PM UTC

Hello @Thatseasy 

If I'm not mistaken, you are working with the Secure Manager. In this context, the DA's permissions do not allow reopening the debug for the secure domain. Even if you change the DA's permissions, they will not be taken into account.

You may observe in your traces "discovery: permission if authorized" -> It depends on the configuration.

In TZ-Closed, there is no need to reopen the debug for the nonsecure domain because it is allowed natively.

 

For more information about the product state in the Secure Manager context, please refer to this UM: https://www.st.com/resource/en/user_manual/um3254-secure-manager-for-stm32h573xx-microcontrollers-stmicroelectronics.pdf -> Chapter 6.3 Product state

 

Best regards

Johny

ThatseasyAuthor
Associate III
Feb 27, 2025 11:00 PM UTC

Thank you Johny for your reply.  The problem was that after attaching the debugger to the running image, none of the breakpoints were hit although I am pretty sure the code was executed. It turned out that the symbol did not match, not because of the DA.