Skip to main content
AMuen.1
Visitor II
Feb 19, 2021 7:10 AM UTC
Question

Dear STM32 Community, I am using : STM32H7xx HAL Driver version number V1.9.0 WolfSSL on a STM32H753, Crypto hardware accelerator not working for TLS

I am trying to use AES-GCM with the crypto hardware accelerator the normal Testvectors are working, but when I connect it to openssl the authentication Tag is wrong. Do you have any idea how to fix this? The normal Encryption in ECB is working. If I use the software Version of the authentication Tag the program is working. Is there any problem with the crypto hardware accelerator and TLS. Please help me.

This topic has been closed for replies.

1 reply

Jocelyn RICARD
ST Employee
Feb 24, 2021 6:44 PM UTC

Hello,

For your information, there are 2 examples of mbedTLS/crypto acceleration provided with STM32.

One for H7 but, unfortunately it does not integrate AES GCM and another one in L5 which integrates it.

These are :

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\mbedTLS\Crypto_Selftest\

STM32Cube_FW_L5_V1.3.1\Projects\STM32L562E-DK\Applications\mbedTLS\Crypto_Selftest

Principle is to provide a *alt.c file for the crypto algorythm.

So, you can check gcm_alt in the L5 CubeFW. It is using the HAL CRYP interface so should also work for STM32H7. At least it could give some hints about your issue.

I didn't check tough.

Best regards

Jocelyn