Skip to main content
Dosan
Associate III
August 31, 2023
Solved

Cypher using AES 128 CTR

Hi,

Im trying to encryp using AES 128 CTR but i dont get the same result that online calculators.

Im using this online calculator: https://cryptii.com/pipes/aes-encryption

My code is the next:

uint8_t IVKey[] = {0xDD, 0xF9, 0x11, 0xA6, 0xDD, 0xF9, 0x11, 0xA6, 0xDD, 0xF9, 0x11, 0xA6, 0xDD, 0xF9, 0x11, 0xA6};

	AesDeInit();

	// CTR AES
 hcryp.Instance = AES;
 hcryp.Init.DataType = CRYP_DATATYPE_1B;
 hcryp.Init.KeySize = CRYP_KEYSIZE_128B;
 hcryp.Init.pKey = (uint32_t *)AESKey;
 hcryp.Init.Algorithm = CRYP_AES_CTR;
 hcryp.Init.pInitVect = (uint32_t *)IVKey;

 if (HAL_CRYP_Init(&hcryp) != HAL_OK)
 {
 Error_Handler();
 }

and the AESKey is the next:

const uint8_t AESKey[] =
{0x44, 0x26, 0x44, 0x20, 0x45, 0x6C, 0x65, 0x74, 0x74, 0x72, 0x6F, 0x6E, 0x69, 0x63, 0x61, 0x20
};

My AES function is the next:

int16_t AesEncrypt(char *In,int16_t Len)
{
	uint8_t Buf[16];

	if (Len & 0x0F)					
		Len+=16-(Len & 0x0F);

	if (HAL_CRYP_DeInit(&hcryp)!=HAL_OK)
		Len=0;
	else if (HAL_CRYP_Init(&hcryp)!=HAL_OK)
		Len=0;
	else
	{
		for (int16_t i=Len;i>0;i-=16)				// Encripta paquete
		{
			if (HAL_CRYP_Encrypt(&hcryp,(uint32_t *)In,16,(uint32_t *)Buf,255)!=HAL_OK)
			{
				Len=0;
				break;
			}
			memcpy(In,Buf,16);
			In+=16;
		}
	}

	return Len;
}

and the string insert into the function is

char Message2[] = {0x50, 0x00, 0x30, 0x30, 0x30, 0x30, 0x30, 0x31, 0x01, 0x03, 0x08, 0x20, 0x00, 0x00, 0x00, 0x00};

The result with the online calculator is: 6c 9d 95 e6 9a 75 ed 03 7c a2 81 80 f9 a6 c3 18

The result that im getting is: c4, b0, c3, 8d, 2d, b2, 5b, 20, 89,75, 57 76, 83, 06, be, 1e

My result is wrong t i dont know what am i doing wrong.

Any suggestion?

Thanks,

Best Regards,

This topic has been closed for replies.
Dosan
DosanBest answer
Associate III
September 2, 2023

Hi all,

Its working now.

My problem was that the AESKey and IVKey were declared as uint8_t and works with uint32_t

and both keys must be declared as a global variables, not a local variable.

Thanks,

Best REgards,

11 replies

AA1
Senior III
August 31, 2023

Instead of use CRYP_DATATYPE_1B, use CRYP_DATATYPE_8B.
Also verify if all needed struct fields are initialized.

Tesla DeLorean
Guru
August 31, 2023

Confirming on-line result with C library here, Decrypting in this case, but symmetrical..

KEY
0000 : 44 26 44 20 45 6C 65 74-74 72 6F 6E 69 63 61 20 D&D Elettronica

IV
0000 : DD F9 11 A6 DD F9 11 A6-DD F9 11 A6 DD F9 11 A6 ................

CRYPT-TEXT
0000 : 50 00 30 30 30 30 30 31-01 03 08 20 00 00 00 00 P.000001... ....

PLAIN-TEXT
0000 : 6C 9D 95 E6 9A 75 ED 03-7C A2 81 80 F9 A6 C3 18 l....u..|.......

  

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dosan
DosanAuthor
Associate III
September 1, 2023

How do you get to this result?

Tesla DeLorean
Guru
September 1, 2023

I tested the premise using my AES library, on a PC, because I don't have much trust in on-line calculators, and I don't have a crypto G0 to hand currently. And I haven't enough coffee yet..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dosan
DosanAuthorBest answer
Associate III
September 2, 2023

Hi all,

Its working now.

My problem was that the AESKey and IVKey were declared as uint8_t and works with uint32_t

and both keys must be declared as a global variables, not a local variable.

Thanks,

Best REgards,