Skip to main content
klaus2
Associate III
Oct 28, 2014 4:38 PM UTC
Question

CRC only up to 8kB Flash instead of 16kB

Posted on October 28, 2014 at 17:38

I want to calculate a CRC over the whole Flash Memory (16kB) of a STM32F030F4. I works fine up 8kB. Putting Values >8192 for BufferLength into CRC_CalcBlockCRC(uint32_t pBuffer[], uint32_t BufferLength). The program won't reach Reset GPIO_PIN_1. Tools: Keil 5.1 ST-LinkV2

Any Idea ?

&sharpdefine FLASH_BASE            ((uint32_t)0x08000000) /*!< FLASH base address in the alias region */

GPIOB->BSRR|=GPIO_Pin_1;

CRC_DeInit();

CRC_ResetDR();

uint32_t *pFLASH= (uint32_t *)FLASH_BASE;

test_CRC=CRC_CalcBlockCRC(pFLASH,8192)

GPIOB->BRR|=GPIO_Pin_1;

#crc-stm32f030f4-flash
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Oct 28, 2014 5:19 PM UTC
Posted on October 28, 2014 at 18:19

BufferLength parameter in 32-bit words, not 8-bit bytes, 16KB would be 4096 words

If you exceed the flash on die you'll get a Hard Fault

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
klaus2
klaus2Author
Associate III
Oct 28, 2014 5:44 PM UTC
Posted on October 28, 2014 at 18:44

Debug shows that MCU goes into Hard Fault. Thx for the Hint with Words, but why does the MCU not go into HardFault between 4096-8192 ?

Tesla DeLorean
Guru
Oct 28, 2014 5:47 PM UTC
Posted on October 28, 2014 at 18:47

Because the die has 32KB of FLASH on it?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
klaus2
klaus2Author
Associate III
Oct 28, 2014 5:58 PM UTC
Posted on October 28, 2014 at 18:58

This sounds evident.

Tesla DeLorean
Guru
Oct 28, 2014 6:11 PM UTC
Posted on October 28, 2014 at 19:11

In the world of IC manufacture, testing and marketing, it's common to sell parts at lower ratings, where expensive test time is skipped. The STM32F2 die have 1MB of flash, the ''256KB'' part is cheaper because the time on the tester is significantly reduced.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..