Skip to main content
BILLyTheLiTTle
Associate
Oct 8, 2020 6:40 AM UTC
Question

CRC Calculation for 8-bit values

I am experimenting with CRC Calculation on a STM32F4-Discovery.

As I have seen in the reference manual this MCU is using CRC-32 used in Ethernet. I am also using https://crccalc.com/ (CRC-32/MPEG-2) to validate the results.

I just activate the CRC in CubeMX and this is my source code for 32-bit values:

uint32_t raw_data_32_bit[BUFFER_SIZE] = { 0x00, 0x01, 0x10, 0x1A, 0xAC, 0xC0 };
uint32_t crc_value_32_bit = 0;
uint8_t is_error_32_bit = 1;
 
crc_value_32_bit = HAL_CRC_Calculate(&hcrc, raw_data_32_bit, BUFFER_SIZE);
 if (crc_value_32_bit == expected_crc_value_32_bit) {
	 is_error_32_bit = 0;
 }

which is working like a charm.

Then I would like to do the same for 8-bit values with this code:

uint32_t expected_crc_value_8_bit = 0xA4541FC6;
uint8_t raw_data_8_bit[BUFFER_SIZE] = { 0x00, 0x01, 0x10, 0x1A, 0xAC, 0xC0 };
uint32_t crc_value_8_bit = 0;
uint8_t is_error_8_bit = 1;
 
crc_value_8_bit = HAL_CRC_Calculate(&hcrc, (uint32_t *) raw_data_8_bit, BUFFER_SIZE); // returns 0xe7206456
 if (crc_value_8_bit == expected_crc_value_8_bit) {
	 is_error_8_bit = 0;
 }

but it returns a different result from the result returns from https://crccalc.com/. The only way to make it work is to create a new 32-bit array using this code:

uint32_t data [BUFFER_SIZE];
for (uint8_t i = 0; i < BUFFER_SIZE; i++)
 data[i] = raw_data_8_bit[i];
 
 
crc_value_8_bit = HAL_CRC_Calculate(&hcrc, data, BUFFER_SIZE); 
if (crc_value_8_bit == expected_crc_value_8_bit) {
 is_error_8_bit = 0;
}

Could someone explain why the 8-bit returns something different from the expected? What am I doing wrong?

This topic has been closed for replies.

7 replies

waclawek.jan
Super User
Oct 8, 2020 7:28 AM UTC

In the first case, you calculate CRC from an array of {0x1A100100, 0xqqqqC0AC, 0xqqqqqqqq, 0xqqqqqqqq, 0xqqqqqqqq, 0xqqqqqqqq}, where qq are whatever bytes happen to be in the memory just after raw_data_8_bit[].

In the second case, you calculate CRC from {0x00000000, 0x000000001, 0x00000010, 0x0000001A, 0x000000AC, 0x000000C0}

Tesla DeLorean
Guru
Oct 8, 2020 9:31 AM UTC

+1

sizeof() the arrays is different, the function is taking a word count, not a byte count.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BILLyTheLiTTle
Associate
Oct 8, 2020 10:08 AM UTC

@Community member​ 

I thought that the conversion

(uint32_t *) raw_data_8_bit

converts the pointer of an 8-bit value into a 32-bit value pointer.

Maybe I have not understand something in pointer functionality. If you could, I would like a more detailed explanation or even some keywords for a google search in order to read an article.

@Community member​ 

Wow! So, is there any way (apart from the third code snippet) to calculate CRC on an 8-bit array?

In this video here, it seems it is working as expected!

@everyone

Thank you for your time.

waclawek.jan
Super User
Oct 9, 2020 6:21 AM UTC

In C, information on variable's *type* is *not* passed to the called function. Rather, the value passed is used according to whatever type is declared for that parameter in the function's declaration.

JW

Gumer RoMa
Visitor II
Feb 4, 2022 1:17 AM UTC

I think you should initialize the CRC using the right parameters for a 8 bit CRC.

Here is an example:

HAL_StatusTypeDef CRC_configure_CDMA2000(){

hcrc.Instance = CRC;

hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_DISABLE;

hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;

hcrc.Init.GeneratingPolynomial = 0x9b;

hcrc.Init.CRCLength = CRC_POLYLENGTH_8B;

hcrc.Init.InitValue = 0xff;

hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;

hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;

hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;

return HAL_CRC_Init(&hcrc);

}

And then use the CRC as follows:

uint8_t crc_data[4] = {0x1A, 0x2B, 0x3C,0x4D};

uint32_t crc_result;

crc_result = HAL_CRC_Calculate(&hcrc, (uint32_t*)crc_data, 4);

Hope this helps,

Gumer

Tesla DeLorean
Guru
Feb 4, 2022 5:17 AM UTC

The thread is over a year old, and discusses a STM32F4 part that doesn't support a programmable CRC peripheral, so only ST's 32-bit one.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..