Skip to main content
AStre
Associate III
Dec 5, 2025 6:28 PM UTC
Solved

Connection STM32L496 read-Out Protection

Hello,

 

I'm posting a new message because the previous one was not answered with successful connection. 

The problem is that when MCU is populated on my board with Read-Our Protection enabled, it is not possible to connect STM32CubeProgrammer v.2.21.0 to that MCU, it becomes a brick.

This option was available in the version 2.0.0. that doesn't work on Windows 11.

How can be done two step connection: 1) full erase and 2) connection ?

 

Thanks,

Alex

TDK
TDKBest answer
Dec 5, 2025 7:26 PM UTC

You marked an answer in your previous thread. Don't mark an answer if it isn't solved.

Solved: STM32CubeProgrammer connection to MCU that has rea... - STMicroelectronics Community

 

 

Why can't you connect to the chip? What happens when you try? Show relevant error messages and screenshots to show the problem.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Dec 5, 2025 7:26 PM UTC

You marked an answer in your previous thread. Don't mark an answer if it isn't solved.

Solved: STM32CubeProgrammer connection to MCU that has rea... - STMicroelectronics Community

 

 

Why can't you connect to the chip? What happens when you try? Show relevant error messages and screenshots to show the problem.

"If you feel a post has answered your question, please click ""Accept as Solution""."
AStre
AStreAuthor
Associate III
Dec 16, 2025 4:00 PM UTC

Hello,

The MCU is soldered on my board and I have access only to UART. The CubeProgrammer v2.21.0 on Windows  11 reports the following error. The old v2.0.0 on Windows 10 allow to make two steps: full erase and connect.

Unfortunately, the version 2.0.0. doesn't work on Windows 11.

Is this option available in CubeProgrammer v2.21.0 ?

Thanks,

Alex