Skip to main content
Associate
May 26, 2025 5:46 PM UTC
Question

Cannot program option bytes on STM32L562 (STM32L562E-DK)

I am trying to run the Secure Boot examples from STM32CubeL5 and have everything built, but on step 2 where I run `TFM_SBSFU_Boot\STM32CubeIDE\regression.sh` I am having an error where I cannot program the option bytes.(Another similar thread was with someone who bought a counterfeit part so I'll also mention that I bought the kit from ST.)

This is the script output

$ ./regression.sh 
regression script started
Regression to RDP 0, enable tz
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.19.0 
 -------------------------------------------------------------------

ST-LINK SN : 004600313137510B33333639
ST-LINK FW : V3J13M4
Board : STM32L562E-DK
Voltage : 3.29V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : --


UPLOADING OPTION BYTES DATA ...

 Bank : 0x00
 Address : 0x50022040
 Size : 40 Bytes

[==================================================] 100% 

 Bank : 0x01
 Address : 0x50022060
 Size : 16 Bytes

[==================================================] 100% 


PROGRAMMING OPTION BYTES AREA ...
Warning: Option Byte: rdp, value: 0xAA, was not modified.
Warning: Option Byte: tzen, value: 0x1, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded
Time elapsed during option Bytes configuration: 00:00:00.003
Remove bank1 protection
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.19.0 
 -------------------------------------------------------------------

ST-LINK SN : 004600313137510B33333639
ST-LINK FW : V3J13M4
Board : STM32L562E-DK
Voltage : 3.29V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : --


Hard reset is performed

UPLOADING OPTION BYTES DATA ...

 Bank : 0x00
 Address : 0x50022040
 Size : 40 Bytes

[==================================================] 100% 

 Bank : 0x01
 Address : 0x50022060
 Size : 16 Bytes

[==================================================] 100% 


PROGRAMMING OPTION BYTES AREA ...
Warning: Option Byte: secwm1_pend, value: 0x0, was not modified.
Warning: Option Byte: wrp1a_pend, value: 0x0, was not modified.
Warning: Option Byte: wrp1b_pend, value: 0x0, was not modified.

 Bank : 0x00
 Address : 0x50022040
 Size : 40 Bytes



Reconnecting...
Reconnected !


UPLOADING OPTION BYTES DATA ...

 Bank : 0x00
 Address : 0x50022040
 Size : 40 Bytes

[==================================================] 100% 

 Bank : 0x01
 Address : 0x50022060
 Size : 16 Bytes

[==================================================] 100% 

OPTION BYTE PROGRAMMING VERIFICATION:

Error: Expected value for Option Byte "secwm1_pend": 0x0, found: 0x75
Error: Expected value for Option Byte "secwm1_pstrt": 0x7F, found: 0x0
Error: Expected value for Option Byte "wrp1a_pend": 0x0, found: 0x23
Error: Expected value for Option Byte "wrp1a_pstrt": 0x7F, found: 0x4
Error: Option Byte Programming failed Or modified by application after OB_LAUNCH

Time elapsed during option Bytes configuration: 00:00:02.122
regression script failed, press a key

If I open STM32CubeProrammer and edit the fields manually I get the same errors.

12:35:55 : UPLOADING OPTION BYTES DATA ...
12:35:55 : Bank : 0x00
12:35:55 : Address : 0x50022040
12:35:55 : Size : 40 Bytes
12:35:55 : Bank : 0x01
12:35:55 : Address : 0x50022060
12:35:55 : Size : 16 Bytes
12:35:55 : OPTION BYTE PROGRAMMING VERIFICATION:
12:35:55 : Error: Expected value for Option Byte "SECWM1_PEND": 0x0, found: 0x75
12:35:55 : Error: Expected value for Option Byte "WRP1A_PEND": 0x0, found: 0x23
12:35:55 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
12:35:55 : Time elapsed during option Bytes configuration: 00:00:02.124
12:40:06 : Disconnected from device.

What can I do to be able to program these bytes?

This topic has been closed for replies.