Skip to main content
Arno1
Senior
Feb 24, 2021 3:23 PM UTC
Solved

Can OTFDEC be used regardless of OCTOSPI modes and interfaces?

We are planning to use an external flash memory connected via QuadSPI to the OCTOSPI peripheral of a STM32H735 (at a later stage that would be STM32H733).

This will be used to run firmware and store downloaded firmware updates with SBSFU. For that we will need the OTFDEC peripheral to ensure date is encrypted for storage.

What I need to know is whether the Quad SPI interface of OCTOSPI will be able to work with OTFDEC in memory mapped mode? The memory also does not support HyperFlash.

It is my understanding (from AN5050 and AN5281) that OTFDEC and OCTOSPI are independent peripherals in operation but where OTFDEC comes in between OCTOSPI and the AXI bus so it should be possible.

This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Feb 24, 2021 6:29 PM UTC

Hello Arno,

yes, it is possible to use OCTOSPI peripheral in QUADSPI mode with OTFDEC without issues.

The OCTOSPI can operate in different bus configurations (single, dual, quad and octo).

Best regards

Jocelyn

2 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Feb 24, 2021 6:29 PM UTC

Hello Arno,

yes, it is possible to use OCTOSPI peripheral in QUADSPI mode with OTFDEC without issues.

The OCTOSPI can operate in different bus configurations (single, dual, quad and octo).

Best regards

Jocelyn

Doug Barnes
Associate II
Mar 20, 2025 4:48 PM UTC

Thank you for the reply, I was wondering the same thing.

A couple follow-up questions if you don't mind:

(1)

Is it the same operation (OTFDEC via OCTOSPI with QuadFlash) with both H5 and U5?  (Wondering if same hardware design & firmware work when moving between H5 and U5, or if H/W interface and firmware and significantly different)

(2)

With OTFDEC through OCTOSPI, is it required to use 2x QUAD-SPI, or can a single QUAD-SPI chip be used if bandwidth / throughput isn't a concern.  I think I've seen that 2x QUAD-SPI chips must be used (for OTFDEC) but I wanted to confirm if that is true.

Thank you!!  (By the way you also provided me with a very helpful answer regarding the PKA on the 'L562 several years ago)