Skip to main content
lovesc1
Associate
Dec 17, 2014 1:50 AM UTC
Question

Can i use IAR or MDK IDE programming the protection option byte (RDP) to Level 0?

Posted on December 17, 2014 at 02:50

In my stm32f405 level 1 is active.I can't updata mcu flash.I need change

RDP to level 0 to reprogram.

Anyone can help me?

thanks.

#stm32f4-rdp
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Dec 17, 2014 5:24 AM UTC
Posted on December 17, 2014 at 06:24

If you have access to a serial port (USART1 or USART3) and the BOOT0 pin you could consider using the System Loader, and the Flash Loader Demonstrator.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
lovesc1
lovesc1Author
Associate
Dec 17, 2014 9:11 AM UTC
Posted on December 17, 2014 at 10:11

Thanks for you reply.

the problem has been solved.

Program code runing from internal RAM or ST-LINK utility can

solve

this problem.