Skip to main content
Phil242
Associate
Jun 23, 2020 11:11 PM UTC
Question

Auto-detecting comport scripts doesn't works (fix inside)

Hello,

On my setup impossible to run the 2 scripts auto-detecting the COMPORT of the current plugged board. Wrong COMPORT is returned and the Teraterm macro crash.

I've patched the original scripts to ask you for the COMPORT. Modified files StartTTPL4.bat and StartTTPL5.bat are here: https://github.com/Phil242/STM32-Security-Workshop

You need to drop them in folder C :\STM32SecuWS\Tools\teraterm and that's it.

Regards,

Philippe

    This topic has been closed for replies.

    13 replies

    Frantz LEFRERE
    ST Technical Moderator
    Jun 24, 2020 6:15 AM UTC

    Thanks for you contribution, to investigate this issue" Wrong COMPORT" which value was return in your case ?

    Phil242
    Phil242Author
    Associate
    Jun 24, 2020 6:47 AM UTC

    I think the enumerator in the "FOR" is getting other things than serials ports.

    The "call :getport COMPORT" return the value "850". I'm running a Win7 64bits French.

    I did not really investigate the problem, just focus on a quick-fix to complete all the pre-workshop tests before the 26 and the best option was to enter COMPORT manually.

    BTW: Another tool who can change your life during development: PopCom ( https://github.com/avishorp/PopCom/releases ). When you insert or remove an USB / COM device, it display a popup with the COM number. A little drawback: there is a little CPU-hogging when the tool is running, but I can live with it on an old core i5 CPU, so it's not really anoying.

    Hope it helps.

    Frantz LEFRERE
    ST Technical Moderator
    Jun 24, 2020 11:15 AM UTC

    Issue is probably coming from the return value of "mode" bash command...

    In the file : C:\STM32SecuWS\Tools\teraterm\StartTTPL4.bat  and C:\STM32SecuWS\Tools\teraterm\StartTTPL5.bat

    replace line

      FOR /F "tokens=4 USEBACKQ" %%F IN (`mode`) DO (

    by

      FOR /F "tokens=4 USEBACKQ" %%F IN (`mode ^| find "Status for device COM"`) DO (

    Any feedback is welcome, as I can't reproduce the issue.

    Phil242
    Phil242Author
    Associate
    Jun 24, 2020 11:38 AM UTC

    Here is the output with the modifier "for":

    C:\STM32SecuWS\Tools\teraterm>StartTTPL4-V2.bat

    Return : COMPORT

    comport : 850

    C:\STM32SecuWS\Tools\teraterm>C:\STM32SecuWS\Tools\teraterm\\ttpmacro.exe C:\STM32SecuWS\Tools\teraterm\\ttlMacro_Startup_L4.ttl 850

    C:\STM32SecuWS\Tools\teraterm>goto end

    C:\STM32SecuWS\Tools\teraterm>endlocal

    C:\STM32SecuWS\Tools\teraterm>Rem

    C:\STM32SecuWS\Tools\teraterm>

    Same problem, but less output, the added "find" as done some filtering.

    Here is an output without the "@echo off":

    C:\STM32SecuWS\Tools\teraterm>StartTTPL4-V2.bat

    C:\STM32SecuWS\Tools\teraterm>Rem @echo off

    C:\STM32SecuWS\Tools\teraterm>setlocal

    C:\STM32SecuWS\Tools\teraterm>SET MYSCRIPT=StartTTPL4-V2.bat

    C:\STM32SecuWS\Tools\teraterm>Rem echo on

    C:\STM32SecuWS\Tools\teraterm>SET DIR_MYSCRIPT=C:\STM32SecuWS\Tools\teraterm\

    C:\STM32SecuWS\Tools\teraterm>call :getport COMPORT

    C:\STM32SecuWS\Tools\teraterm>FOR /F "tokens=4 USEBACKQ" %F IN (`mode | find "Status for device COM"`) DO (

    echo %F

     if %F NEQ CON: SET COMPORT=%F

    )

    C:\STM32SecuWS\Tools\teraterm>echo Return : COMPORT

    Return : COMPORT

    C:\STM32SecuWS\Tools\teraterm>GOTO :EOF

    C:\STM32SecuWS\Tools\teraterm>if "850" == "" goto ErrorCOM

    C:\STM32SecuWS\Tools\teraterm>if "850" == "CON:" goto ErrorCOM

    C:\STM32SecuWS\Tools\teraterm>SET TT_MACRO_FILE=C:\STM32SecuWS\Tools\teraterm\\ttlMacro_Startup_L4.ttl

    C:\STM32SecuWS\Tools\teraterm>SET TT_MACRO_EXE=C:\STM32SecuWS\Tools\teraterm\\ttpmacro.exe

    C:\STM32SecuWS\Tools\teraterm>echo comport : 850

    comport : 850

    C:\STM32SecuWS\Tools\teraterm>C:\STM32SecuWS\Tools\teraterm\\ttpmacro.exe C:\STM32SecuWS\Tools\teraterm\\ttlMacro_Startup_L4.ttl 850

    C:\STM32SecuWS\Tools\teraterm>goto end

    C:\STM32SecuWS\Tools\teraterm>endlocal

    C:\STM32SecuWS\Tools\teraterm>Rem

    The COM55: (my current COMPORT for the plugged board) is missing, meaning the "find" is too restrictive.

    Here is a full dump with the original script:

    C:\STM32SecuWS\Tools\teraterm>StartTTPL4.bat

    C:\STM32SecuWS\Tools\teraterm>Rem @echo off

    C:\STM32SecuWS\Tools\teraterm>setlocal

    C:\STM32SecuWS\Tools\teraterm>SET MYSCRIPT=StartTTPL4-V2.bat

    C:\STM32SecuWS\Tools\teraterm>Rem echo on

    C:\STM32SecuWS\Tools\teraterm>SET DIR_MYSCRIPT=C:\STM32SecuWS\Tools\teraterm\

    C:\STM32SecuWS\Tools\teraterm>call :getport COMPORT

    C:\STM32SecuWS\Tools\teraterm>FOR /F "tokens=4 USEBACKQ" %F IN (`mode`) DO (

    echo %F

     if %F NEQ CON: SET COMPORT=%F

    )

    C:\STM32SecuWS\Tools\teraterm>(

    echo COM3:

     if COM3: NEQ CON: SET COMPORT=COM3:

    )

    COM3:

    C:\STM32SecuWS\Tools\teraterm>(

    echo 8

     if 8 NEQ CON: SET COMPORT=8

    )

    8

    C:\STM32SecuWS\Tools\teraterm>(

    echo COM5:

     if COM5: NEQ CON: SET COMPORT=COM5:

    )

    COM5:

    C:\STM32SecuWS\Tools\teraterm>(

    echo 8

     if 8 NEQ CON: SET COMPORT=8

    )

    8

    C:\STM32SecuWS\Tools\teraterm>(

    echo COM6:

     if COM6: NEQ CON: SET COMPORT=COM6:

    )

    COM6:

    C:\STM32SecuWS\Tools\teraterm>(

    echo 8

     if 8 NEQ CON: SET COMPORT=8

    )

    8

    C:\STM32SecuWS\Tools\teraterm>(

    echo COM4:

     if COM4: NEQ CON: SET COMPORT=COM4:

    )

    COM4:

    C:\STM32SecuWS\Tools\teraterm>(

    echo 8

     if 8 NEQ CON: SET COMPORT=8

    )

    8

    C:\STM32SecuWS\Tools\teraterm>(

    echo COM55:

     if COM55: NEQ CON: SET COMPORT=COM55:

    )

    COM55:

    C:\STM32SecuWS\Tools\teraterm>(

    echo 8

     if 8 NEQ CON: SET COMPORT=8

    )

    8

    C:\STM32SecuWS\Tools\teraterm>(

    echo CON:

     if CON: NEQ CON: SET COMPORT=CON:

    )

    CON:

    C:\STM32SecuWS\Tools\teraterm>(

    echo 850

     if 850 NEQ CON: SET COMPORT=850

    )

    850

    C:\STM32SecuWS\Tools\teraterm>echo Return : COMPORT

    Return : COMPORT

    C:\STM32SecuWS\Tools\teraterm>GOTO :EOF

    C:\STM32SecuWS\Tools\teraterm>if "850" == "" goto ErrorCOM

    C:\STM32SecuWS\Tools\teraterm>if "850" == "CON:" goto ErrorCOM

    C:\STM32SecuWS\Tools\teraterm>SET TT_MACRO_FILE=C:\STM32SecuWS\Tools\teraterm\\ttlMacro_Startup_L4.ttl

    C:\STM32SecuWS\Tools\teraterm>SET TT_MACRO_EXE=C:\STM32SecuWS\Tools\teraterm\\ttpmacro.exe

    C:\STM32SecuWS\Tools\teraterm>echo comport : 850

    comport : 850

    C:\STM32SecuWS\Tools\teraterm>C:\STM32SecuWS\Tools\teraterm\\ttpmacro.exe C:\STM32SecuWS\Tools\teraterm\\ttlMacro_Startup_L4.ttl 850

    C:\STM32SecuWS\Tools\teraterm>goto end

    C:\STM32SecuWS\Tools\teraterm>endlocal

    C:\STM32SecuWS\Tools\teraterm>Rem

    C:\STM32SecuWS\Tools\teraterm>

    Sorry to not dig a little more, but this evening I'll look deeper. Maybe with those traces you can have more clues to spot the problem.

    (but keep in mind the problem is -badly- solved by entering the port number by hand and that'll not stop me for Friday 26).

    Jocelyn RICARD
    ST Employee
    Jun 24, 2020 12:04 PM UTC

    Hello Phil,

    could you please give the output of mode command ?

    Thank you

    Best regards

    Jocelyn

    Phil242
    Phil242Author
    Associate
    Jun 24, 2020 12:11 PM UTC

    Here it is:

    C:\STM32SecuWS\Tools\teraterm>mode

    Statut du périphérique COM3:

    ----------------------------

       Baud :           115200

       Parité :         None

       Bits de données : 8

       Bits d'arrêt :   1

       Temporisation :  OFF

       XON/XOFF :       OFF

       Protocole CTS :  OFF

       Protocole DSR :  OFF

       Sensibilité DSR : OFF

       Circuit DTR :    OFF

       Circuit RTS :    OFF

    Statut du périphérique COM5:

    ----------------------------

       Baud :           0

       Parité :         None

       Bits de données : 8

       Bits d'arrêt :   1

       Temporisation :  OFF

       XON/XOFF :       OFF

       Protocole CTS :  OFF

       Protocole DSR :  OFF

       Sensibilité DSR : OFF

       Circuit DTR :    OFF

       Circuit RTS :    OFF

    Statut du périphérique COM6:

    ----------------------------

       Baud :           0

       Parité :         None

       Bits de données : 8

       Bits d'arrêt :   1

       Temporisation :  OFF

       XON/XOFF :       OFF

       Protocole CTS :  OFF

       Protocole DSR :  OFF

       Sensibilité DSR : OFF

       Circuit DTR :    OFF

       Circuit RTS :    OFF

    Statut du périphérique COM4:

    ----------------------------

       Baud :           0

       Parité :         None

       Bits de données : 8

       Bits d'arrêt :   1

       Temporisation :  OFF

       XON/XOFF :       OFF

       Protocole CTS :  OFF

       Protocole DSR :  OFF

       Sensibilité DSR : OFF

       Circuit DTR :    OFF

       Circuit RTS :    OFF

    Statut du périphérique COM55:

    -----------------------------

       Baud :           0

       Parité :         Odd

       Bits de données : 8

       Bits d'arrêt :   1

       Temporisation :  OFF

       XON/XOFF :       OFF

       Protocole CTS :  OFF

       Protocole DSR :  OFF

       Sensibilité DSR : OFF

       Circuit DTR :    OFF

       Circuit RTS :    ON

    Statut du périphérique CON:

    ---------------------------

       Lignes :         2260

       Colonnes :       160

       Vitesse clavier : 31

       Délai clavier :  1

       Page de codes :  850

    C:\STM32SecuWS\Tools\teraterm>

    The Nucleo-L476 is port "COM55:".

    Jocelyn RICARD
    ST Employee
    Jun 24, 2020 12:39 PM UTC

    Hi Phil,

    ok thank you. I could debug the issue.

    Issue comes from the very last line that is different in french =)

    So, the good fix should be:

    In the 2 files:

    C:\STM32SecuWS\Tools\teraterm\StartTTPL4.bat

    C:\STM32SecuWS\Tools\teraterm\StartTTPL5.bat

    replace line

      FOR /F "tokens=4 USEBACKQ" %%F IN (`mode`) DO (

    by

      FOR /F "tokens=4 USEBACKQ" %%F IN (`mode ^| find " COM"`) DO (

      

    Best regards

    Jocelyn

    RDien
    Associate III
    Nov 12, 2020 1:16 AM UTC

    Doesn't work as well for me. Managed to launch manually.

    Frantz LEFRERE
    ST Technical Moderator
    Nov 12, 2020 5:59 AM UTC
    Phil242
    Phil242Author
    Associate
    Jun 24, 2020 7:07 PM UTC

    So, this last one was the good one !

    Sorry to not investigate more, but I was out of time this whole day ...

    I have update the GitHub with 2 working scripts and 2 other in fallback mode, asking you for the COMPORT:

    https://github.com/Phil242/STM32-Security-Workshop

    Thanks for the support, see you friday.

    Philippe

    Frantz LEFRERE
    ST Technical Moderator
    Nov 12, 2020 3:00 PM UTC

    -