Skip to main content
JSim
Visitor II
Oct 15, 2019 8:55 PM UTC
Question

Are these vulnerabilities possible or have been acknowledged: https://www.cvedetails.com/vulnerability-list/vendor_id-1726/year-2019/ST.html Thanks in advance.

If the Read Protection is set to RDP Level 1 in the Option Bytes, does the above claimed vulnerabilities affect STM32F7xx or STM32H7xx MCUs?

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
Oct 16, 2019 12:20 AM UTC

> If the Read Protection is set to RDP Level 1 in the Option Bytes, does the above claimed vulnerabilities affect STM32F7xx or STM32H7xx MCUs?

That's a question you should ask the authors of the given paper:

Marc Schink

Fraunhofer Institute AISEC

marc.schink@aisec.fraunhofer.de

Johannes Obermaier

Fraunhofer Institute AISEC

johannes.obermaier@aisec.fraunhofer.de

The paper does not mention either level of RDP. They deal with PCROP, which is something different.

They don't even acknowledge existence of RDP, which is sort of unfair, but then it would decrease the sensational value of their paper.

JW