Skip to main content
Visitor II
September 21, 2026
Solved

Alternatives to STM32HSM-V2 for STM32H573 secure programming at external CM?

  • September 21, 2026
  • 1 reply
  • 66 views

Hello,

We are going to use the STM32H573 MCU (STM32H573IIK3Q) on our board, and we are now preparing for mass production. Production will be done at an external contract manufacturer (not in-house), and we need to provision keys and firmware securely during programming.

My main question: Is the STM32HSM-V2 card strictly required for secure programming at high volume, or are there supported alternatives?

Specifically:

1. As far as I understand, the SFI license mechanism is tied to ST's key hierarchy inside the ROM bootloader, so a third-party/commercial HSM (Thales, nShield, etc.) cannot generate licenses that the chip will accept. Is that correct, or is there any supported way to run SFI with our own HSM infrastructure instead of the ST smartcard?

2. If STM32HSM-V2 is the only option: for volumes well beyond 300 units, V2ML (10K) and V2HL (100K) do not seem to be orderable through distributors. Is the intended path to request them through an ST sales office, and what lead time should we plan for?

3. Our CM uses gang programmers rather than a per-device STM32CubeProgrammer + ST-LINK station. What is the recommended way to integrate SFI into third-party gang programmers (Data I/O, BPM, etc.)? Does the HSM card need to be physically attached to each programming station, and is there a list of programmer vendors with validated SFI support for the H5 series?

Environment: STM32H573IIK3Q, STM32CubeProgrammer (latest), STM32HSM-V2, external CM.

Thank you in advance.

Best answer by Jocelyn RICARD

Hello ​@obrahimo,

Unfortunately, SFI is not able to use any external HSM to generate the license.

For STM32HSM-V2 availability, there is an action ongoing to make it available but for high volumes I confirm this is much better to contact the sales office.

Regarding SFI support by programmer, we have a partnership program to provide necessary documentation to allow the implementation of the SFI programming sequence. Behind this, it is possible to implement a kind of license server using STM32HSM-V2 that receives the certificate if a chip from one programmer and provide the license in return.  

Best regards

Jocelyn

1 reply

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
September 22, 2026

Hello ​@obrahimo,

Unfortunately, SFI is not able to use any external HSM to generate the license.

For STM32HSM-V2 availability, there is an action ongoing to make it available but for high volumes I confirm this is much better to contact the sales office.

Regarding SFI support by programmer, we have a partnership program to provide necessary documentation to allow the implementation of the SFI programming sequence. Behind this, it is possible to implement a kind of license server using STM32HSM-V2 that receives the certificate if a chip from one programmer and provide the license in return.  

Best regards

Jocelyn