Question
About OEMiROT_Appli_TrustZone for H563ZIT6 SBSFU
- 2 replies
- 174 views
Hi,
I use OEMiROT_Appli_TrustZone +OEMiROT_Boot to do some change in order to migrate to my project.
Version: STM32Cube_FW_H5_V1.5.0
1.i change the secure image and non secure image size in flash_layout.h from OEMiROT_Boot.
#define FLASH_S_PARTITION_SIZE (0x20000) /* 128KB for S partition */
#if defined(DEVICE_1M_FLASH_ENABLE)
#define FLASH_NS_PARTITION_SIZE (0x30000) /* 192 KB for NS partition */
#else
#define FLASH_NS_PARTITION_SIZE (0x60000) /* 384 KB for NS partition */
2.then rebuild the OEMiROT_Boot.
it will autocratically change the ld file and image.xls size of OEMiROT_Appli_TrustZone.
3.rebuild OEMiROT_Appli_TrustZone secure ap and non secure app
4.execute STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI\ROT_Provisioning\OEMiROT\provisioning.bat OK
5.reconnet the board with UART . it shows the error as follow:.
INF] TAMPER Activated
[INF] BANK 1 secure flash 0, 27] : OB [0, 14]
[ERR] Unexpected value for secure flash protection