Skip to main content
repzak
Associate II
Feb 19, 2010 6:27 AM UTC
Question

ZeroG

Posted on February 19, 2010 at 07:27

ZeroG

    This topic has been closed for replies.

    8 replies

    repzak
    repzakAuthor
    Associate II
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    Hello,

    Actually quite simple, the datasheet with registers,etc are not released to public, and the driver for the ZeroG module is licensed to microchip now and may only be used in microchip controllers.

    Then there will be some hard work to make you own driver when you don't have any datasheet.

    Kasper

    Andrew Neil
    Super User
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    Why would it make a difference?

    I'm sure people used to use Microchip's ehternet chips before STM32's were available with onboard ethernet.

    And I'm sure people will continue to use other Microchip products...
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    No, that's not true.

    You can create an account exactly as before by clicking the 'Create a New Account' button at 

    http://support.zerogwireless.com/ics/support/default.asp?deptID=5560

    It is quite common for manufacturers to require registration in order to gain access to Datasheets, etc.

    The 'Copyright' section of their Terms of  Use does seem bizarrely stupid, though!
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    repzak
    repzakAuthor
    Associate II
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    Hello,

    could you please then share the link/file, because my account only gives access to the electrical datasheet and nothing about the protocol/register/setup etc.

    Kasper

    repzak
    repzakAuthor
    Associate II
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    Hello,

    Yes i found that library ''WiShield'' if that is the one?..

    I allready converted that into my code and properly going to test that today, only need to solder some wires on a ZeroG module to test it.

    But i think this driver is very primitive also, it can not search for the AP and so... but first i need to verify it can work atleast before i desgin my board.

    Kasper

    tkjmail2
    Associate III
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    I'm already working on this, porting the ZeroG code from an AVR Library I've made earlier... And this isn't difficult, as the code is in C too, so I only have to change the SPI routines, and some of the variable definitions!

    I will return to you if I manage to get it working.

    Best Regards

    Thomas Jespersen

    repzak
    repzakAuthor
    Associate II
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    Hello,

    I got it up running in Keil with their TCP/IP stack and dynamic ram allocation.

    I just need to try to eliminate the need for copy the entire packet as done in the original driver, that is a of time wasted.

    you can contact me through 

    mailto:zerog.wifi@gmail.com

      to get a copy, and then maybe we both can work to make the best solution for optimization.

    Kasper

    tkjmail2
    Associate III
    May 17, 2011 11:40 AM UTC
    Posted on May 17, 2011 at 13:40

    Yeah, that's the one!

    If you get it running before I do, please leave me a message :)

    Thomas