Skip to main content
lowpowermcu
Associate III
August 9, 2010
Question

Ymodem transmit function

  • August 9, 2010
  • 1 reply
  • 559 views
Posted on August 09, 2010 at 10:17

Ymodem transmit function

    This topic has been closed for replies.

    1 reply

    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 14:01

    One of the main reasons for using Y-MODEM (or X-MODEM) is that it is supported by just about every terminal application or serial comms library around - so it's very rare that you actually need to implement it yourself!

    However, if you really do need to implement it yourself, it's not difficult - see: 

    http://www.techheap.com/communication/modems/xmodem-ymodem_reference.html

     for the protocol details

    Also: 

    http://www.techheap.com/communication/modems/xmodem.html

    And: 

    http://en.wikipedia.org/wiki/XMODEM

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.