Skip to main content
dps
Associate
Feb 12, 2009 3:50 AM UTC
Question

X value of BOOT1 pin

Posted on February 12, 2009 at 04:50

X value of BOOT1 pin

    This topic has been closed for replies.

    2 replies

    dps
    dpsAuthor
    Associate
    May 17, 2011 11:02 AM UTC
    Posted on May 17, 2011 at 13:02

    Hello.

    I want to start application from User Flash memory.

    I must connect BOOT_0 pin to log. 0............. OK

    But, is it possible to connect BOOT1 pin to log. 0, too ?

    In datasheet's table it is state ''X'' for BOOT_1 pin and log.0 for BOOT0_0 pin.

    What ''X'' mean ?

    1. Unconnected float pin (Hi-Z)

    or

    2. don´t care (log.1 or log.0)

    Is it possible to run application from User Flash memory with this configuration: BOOT_0 = log. 0, BOOT_1 = log.0 ?

    Thanks

    jilisegiar
    Associate III
    May 17, 2011 11:02 AM UTC
    Posted on May 17, 2011 at 13:02

    it means don't care