Skip to main content
yang hong
Associate III
May 23, 2018 2:45 PM UTC
Question

x-nucleo-plc01a1

Posted on May 23, 2018 at 16:45

Hello, 

I am trying x-nucleo-plc01a1. but there are two jumpers (J5 and J11) on the board. I can't find any document to describe how to use them. Anybody can help?

thank you.

    6 replies

    ST Technical Moderator
    May 24, 2018 1:41 PM UTC
    Posted on May 24, 2018 at 15:41

    Hello

    yang

    ,

    You have to review theX-NUCLEO-PLC01A1 schematic in the

    http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/9c/25/64/62/4f/bc/4d/9f/DM00213568/files/DM002135pdf/jcr:content/translations/en.DM002135pdf

    Getting started with the X-NUCLEO-PLC01A1.

    You mayrefer to the

    http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/2a/5b/7c/a9/ee/27/42/dd/DM00429687/files/DM004296pdf/jcr:content/translations/en.DM004296pdf

    , there is a figure on page 14

    (Figure 9)

    of theX-NUCLEO-PLC01A1 expansion board shown how the jumpers are configured.

    Best Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    yang hong
    yang hongAuthor
    Associate III
    May 24, 2018 4:00 PM UTC
    Posted on May 24, 2018 at 16:00

    Thank you for your reply. I have some questions about this expansion board:

    1) when I apply 24vdc on terminal block J8 (pin 1 and pin 2), I should have one led on (power good, D24) or this led should not be on , but I don't have it. I check all test points (TP2, TP3, TP5), TP4=24V, TP5=5V, TP2=20V,TP3=2.1V, as soon as I try to talk VNI8200XP, I got faulty led on(D23). Do you have any idea? Thanks a lot.

    Jitendra J
    Associate
    Jun 5, 2018 7:00 AM UTC
    Posted on June 05, 2018 at 07:00

    Hello

    yang

    , faulty LED is attached to VNI8200XP and represents one of the two conditions:

    1. Channel overtemperature (OVT)

    2. Parity check fail when SPI mode is used

    It would be interesting to find out why you don't have power good LED and what causes it to be not on when you apply 24V (you may try to increase current limit of power supply). Also which Nucleo board are you using with X-NUCLEO-PLC01A1.

    Regards,

    Jitendra

    Explorer
    Mar 17, 2025 12:09 PM UTC

    Thank you so much for sharing your knowledge about using the plc010a with the stm32f429zi! I have been searching for this error for many days and almost went crazy!

    Additional note: On the underside of the NUCLEO F429 board, there are two solder bridges that allow you to switch from PA7 to PB5. These are labeled SB121 and SB122.

    Visitor II
    Dec 1, 2025 6:48 AM UTC

    Hey Yang, 

    I am trying to use nucleo stm32f767zi with plc01a1, I am not using X-Cube_PLC1 package, I want to code it using stm32cubeide using SPI, can you tell me the power and requirements of the plc board if i am connecting them externally using wires not stacking on the base board.