Skip to main content
John Koshi
Associate II
Oct 20, 2017 2:17 AM UTC
Solved

X-CUBE-AWS

Posted on October 20, 2017 at 04:17

When I try to add the X-CUBE-AWS expansion library package to my STM32CubeMX (which has been updated to the latest version - 4.22.1) I get the error: 'This package version is not managed on this version of STM32CubeMX'.

I used the drop down menu item under Help -> Install New Libraries in the STM32CubeMX , and pointed to a local copy of the 'en.x-cube-aws.zip' file. Is this the correct way to add the 

X-CUBE-AWS expansion library?

Thanks in advance.

    This topic has been closed for replies.
    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    Oct 20, 2017 9:23 AM UTC
    Posted on October 20, 2017 at 11:23

    Hi

    naturelover

    ‌,

    The X-Cube-AWS package should be used on standalone and cannot be installed with STM32CubeMX.

    You have jsu to download it then run the available examples . You have to refer to

    http://www.st.com/resource/en/user_manual/dm003674pdf

    for details.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

    2 replies

    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    Oct 20, 2017 9:23 AM UTC
    Posted on October 20, 2017 at 11:23

    Hi

    naturelover

    ‌,

    The X-Cube-AWS package should be used on standalone and cannot be installed with STM32CubeMX.

    You have jsu to download it then run the available examples . You have to refer to

    http://www.st.com/resource/en/user_manual/dm003674pdf

    for details.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    John Koshi
    Associate II
    Oct 20, 2017 11:02 PM UTC
    Posted on October 20, 2017 at 23:02

    Hi Amel,

    Thanks for the clarification. I extracted the zip file of the expansion library package,

    and it appears to by intended for Windows users.

    I am using the SW4STM32 IDE under Linux for my development, and I wanted to just

    confirm whether the X-CUBE-AWS package can be used under Linux as well, or not,

    especially since drivers, etc., are provided in the package.

    thanks,

    John