Question
Wrong pin names between the electrical schematic and the user manual for NUCLEO32 boards.
Hello.
I’ve noticed a discrepancy in the documentation. The electrical schematics for the NUCLEO32 board show that D8 is connected to PF0/PC14 and that D7 is connected to PF1/PC15. However UM1956 User manual for STM32 Nucleo-32 boards (MB1180) says throughout the manual that D8 is connected to PF1/PC15 and that D7 is connected to PF0/PC14.