wrong data receive with uart1 on stm32f103rct6
Nowadays. i debug the uart1 under linux with arm-none-eabi- cross compile.
Now i meet a problem,i config uart with 115200 baudrate and 8 databotlen 1 stopbit none parity.use Hsi for SYSCLK APB1 and APB2 CLK BOTH 36MHz. I can receive data from the chip right from the pc console.but when i send some data to the chip.it's mistake .for examplr i input **a** the chip get the value eq **0xa1** always the data is wrong?
I'm curious how could cause the chip tx right but rx wrong?