Question
Wrong clock frequency after IWDG reset [STM32F405]
Posted on April 09, 2016 at 12:42
Hi all,
I'm experiencing a strange problem on STM32F405When a IWDG reset happens, the uC restarts with a wrong clock frequency, I think it's running from HSI instead of HSE. Same problem happens even if I call NVIC_SystemReset()If I power the board or I reset the board using the reset pin everything is working fine.Should I reconfigure something, or it should be a clock startup problem?I'm using this 8MHz xtal () with 22pf load capacitance, and uC frequency should be 168MHz.Any help is really appreciated.Luigi #stm32f405-startup-watchdog-clock