Skip to main content
gurnett2
Associate II
Apr 9, 2013 4:26 PM UTC
Question

Writing to internal Flash

Posted on April 09, 2013 at 18:26

I'm trying to write to the internal flash of a STM32F103ZE. I've been using the following code

FLASH_Unlock();

uint32_t Start=0x8008000;

uint32_t End =0x800C000;

NbrOfPage = (End - Start) / FLASH_PAGE_SIZE;

 

/* Clear All pending flags */

FLASH_ClearFlag(FLASH_FLAG_BSY | FLASH_FLAG_EOP | FLASH_FLAG_PGERR | FLASH_FLAG_WRPRTERR);

 

/* Erase the FLASH pages */

for(EraseCounter=0; EraseCounter<NbrOfPage && (FLASHStatus == FLASH_COMPLETE); EraseCounter++)

{

  FLASHStatus = FLASH_ErasePage(Start + (FLASH_PAGE_SIZE * EraseCounter));

}

uint32_t Address = Start;

while((Address < End) && (FLASHStatus == FLASH_COMPLETE))

    {

        FLASHStatus = FLASH_ProgramWord(Address, Data);

        Address = Address + 4;

    }

    FLASH_Lock();

However, this results in a visit to the hardfault_handler. Are there some other steps required to get this working? I'm using crossworks.

Thanks

-Michael
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    Apr 9, 2013 6:12 PM UTC
    Posted on April 09, 2013 at 20:12

    Doesn't look too objectionable. Make sure you don't erase memory you are currently executing from.

    Diagnose the cause of the Hard Fault, understand the registers and processor state when it faulted. If you understand where, and why, it faulted you'd be in a better position to solve the problem.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..