Skip to main content
TARHAN SAMAH
Senior
May 23, 2018 8:05 AM UTC
Solved

writing half word 16 bits on flash stm32f429ZI

Posted on May 23, 2018 at 10:05

Hello evry body , i can write a byte on flash of stm32f429ZI WİTH success . for info i use nucleo 144 and sector 23 the last sector .

for example :

with these adresses 

uint32_t locip1_adress=0x081E0001;//LAST sector for STM32429ZI sector 23

uint32_t locip2_adress=0x081E0002;//LAST sector for STM32429ZI sector 23

uint32_t locip3_adress=0x081E0003;//LAST sector for STM32429ZI sector 23

uint32_t locip4_adress=0x081E0004;//LAST sector for STM32429ZI sector 23

uint32_t remip1_adress=0x081E0005;//LAST sector for STM32429ZI sector 23

uint32_t remip2_adress=0x081E0006;//LAST sector for STM32429ZI sector 23

uint32_t remip3_adress=0x081E0007;//LAST sector for STM32429ZI sector 23

uint32_t remip4_adress=0x081E0008;//LAST sector for STM32429ZI sector 23

uint32_t ROV_min_adress=0x081E0009;//LAST sector for STM32429ZI sector 23 this data needs two bytes

uint32_t ROV_max_adress=0x081E00B;//LAST sector for STM32429ZI sector 23 this data needs two bytes

/* Unlock the Flash to enable the flash control register access *************/

HAL_FLASH_Unlock();

/* Fill EraseInit structure*/

EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;

EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;

EraseInitStruct.Sector = FLASH_SECTOR_23;

EraseInitStruct.NbSectors = 1;

//you need to erase entire sector before write anything

HAL_FLASHEx_Erase(&EraseInitStruct, &SECTORError);//we need to erase the sector before write

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, locip1_adress,locip1);//write one byte

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, locip2_adress,locip2);//write one byte

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, locip3_adress,locip3);//write one byte

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, locip4_adress,locip4);//write one byte

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, remip1_adress,remip1);//write one byte// we need to write also all other parameter because we delete all sector 23

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, remip2_adress,remip2);//write one byte

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, remip3_adress,remip3);//write one byte

HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, remip4_adress,remip4);//write one byte

HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD,ROV_min_adress,Rover_ID_min[0]);//write one 16 bit

HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD,ROV_max_adress,Rover_ID_max[0]);//write one 16 bit

HAL_FLASH_Lock();

But in THE HALFWORD writing i have prblm with 16 bit writing looks these adresses are not accepted 

uint32_t ROV_min_adress=0x081E0009;  ----> in my idea for one word ill use 0x081E0009+ 0x081E000A Two bytes --->is it right

uint32_t ROV_max_adress=0x081E00B;-----> WİLL use 0x081E000B+0x081E000C  two bytes 

but the data at the reading of  ROV_max_adress are wrong strangely ??

how should i select the adresses separation between them for writing half word can someone give me an example . thanks 

could not find detail about mem data adresses in detail .

    This topic has been closed for replies.
    Tilen MAJERLE
    Tilen MAJERLEBest answer
    ST Employee
    May 24, 2018 2:39 PM UTC
    Posted on May 24, 2018 at 14:39

    Hello

    doumandjisamah

    ‌,

    To know when you have 16-bit aligned address, you can check LSB bit which must be 0, thus:

    • Every address is byte aligned, no matter on LSB bit value
    • Every second address is 16-bit (half-word) aligned

      • 0 = 0b000

        0

        , 2 = 0b001

        0

        , 4 = 010

        0

        , 6 = 0b011

        0

    • Every 4th address is 32-bit (word) aligned, LSB and LSB-1 bits must be 0.

      • 0 = 0b00

        00

        ;4 = 0b01

        00

        ;8 = 0b10

        00

    In your case, address

    0x081E0009

    is odd,

    LSB =1 => not 16-bit aligned, while

    0x081E000A

    or

    0x081E000C

    is even number,

    LSB = 0 => 16-bit aligned.

    If we go back to flash write process:

    • To be able to write in BYTE mode, you may use any valid flash address (LSB don't care)
    • To be able to write in HALF-WORD mode, your address must be 16-bits aligned (LSB must be 0)
    • To be able to write in WORD mode, your address must be 32-bits aligned (LSB and LSB - 1 must be 0)
    • To be able to write in QWORD mode, your address must be 64-bits aligned (LSB, LSB - 1 and LSB - 2 must be 0).

    Hope it is clear now.

    Best regards,

    Tilen

    13 replies

    Tilen MAJERLE
    ST Employee
    May 23, 2018 8:22 AM UTC
    Posted on May 23, 2018 at 10:22

    Dear

    ‌,

    please check FLASH_SR register for possible errors when programming.

    Address must be 16-bits aligned, which is not your case.

    uint32_t ROV_min_adress=0x081E0009;�?

    should be

    uint32_t ROV_min_adress=0x081E0008; //Either 8 and then it will use 8 + 9 bytesuint32_t ROV_min_adress=0x081E000A; //Or A and then it will use A + B bytes�?�?

    Best regards,

    Tilen

    TARHAN SAMAH
    Senior
    May 23, 2018 1:23 PM UTC
    Posted on May 23, 2018 at 13:23

    Hello Mister Tilen , thanks for answering but i think you didnt understand my question , 

     i have two datas to save for example:

    Rover_ID_min[0]=0x0012;

    Rover_ID_max[0]=

    0x0044;

    in these adresses 

    uint32_t ROV_min_adress=0x081E0009;

    uint32_t ROV_min_adress=0x081E000B;

    HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD,ROV_min_adress,Rover_ID_min[0]);//write one 16 bit

     ,------> İLL use 9 and A

     

    HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD,ROV_max_adress,Rover_ID_max[0]);//write one 16 bit

     ----->İLL USE B AND C 

    SO WHY THERE İS A MİSTAKE ON MY READED DATA since i separate wel the adresses 

    Tilen MAJERLE
    ST Employee
    May 23, 2018 1:52 PM UTC
    Posted on May 23, 2018 at 13:52

    Dear

    doumandjisamah

    ‌,

    what are the values you read back in this case?

    Please note, addresses0x081E0009 and0x081E000Bare not 16-bits aligned and you cannot program to these addresses as 16-bits (HALFWORD). You may use addresses0x081E0008

    and

    0x081E000A or

    0x081E000A

    and

    0x081E000C or use byte programming width.

    Best regards,

    Tilen

    chum
    Associate III
    Mar 29, 2019 10:29 AM UTC

    Anyone done with STM32F429ZI LwIP_TFTP_Server application ?

    Using Ethernet i want to transfer file on host server to target board memory or USB.

    I'm using Linux with eclipse IDE, USB with OTG.

    How to done this ?