Skip to main content
Associate
Jan 24, 2025 1:33 PM UTC
Solved

writing flash memory failure

Hi everyone

I'm using a STM32F401RCT6 to control a valve actuator

There is a counter of number of cycles for the actuator (RunTime), and when its value changes, the value of that counter must be stored in the memory for tracking and support.

The actuator is powered by an external power supply and additionally there's a battery in case the power fails.

In some rare cases, the memory storage process is corrupted, and we lose the complete storage values previously saved.

We are trying to replicate the fail, but it is really impossible

Do you have any idea of what can cause that loss of information in the memory and how could we replicate this failure in order to fix the bug

below is part of the code that writes to memory

Thank you very much

 

int WriteToFlash(bool force)
{
uint8_t NibleH=0;
uint8_t NibleL=0;
int16_t AuxData=0;
uint32_t Variable_Guardar;
uint32_t PAGError = 0;
FLASH_EraseInitTypeDef EraseInitStruct;

if((Entrada_Control_Seleccionada!=Problem || force) && Scale.VoltMain >20 ) //Force write in memory when a fail occurs
{
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.Sector = FLASH_SECTOR_1;
EraseInitStruct.NbSectors = 1;
EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;

HAL_FLASH_Unlock();
// Erase the USER_FLASH
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGError) != HAL_OK)
{
return 1;
}
// Write the delay value in flash memory //0x5051
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1, 0x5051) != HAL_OK)
{
return 1;
}

Index.Modo_Entrada=Entrada_Control_Seleccionada_M;
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(0,0,Index.Modo_Entrada,Index.ModeWork);
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+4, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}

AuxData=Scale.Temp_SP;//Save Anticondensation temperature value
NibleL=0xFF & AuxData;
NibleH=AuxData>>8;
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(0,0,NibleH,NibleL);
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+8, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(Index.FactorScal,TEMP_AlmHH,Index.LED,Index.Modo_Giro); //Save setting TEMP_AlmHH
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+12, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(0,0,Index.LED_Update,Index.SP_Fault_Power); //LFH, 2023/05/26 Ver 2.1.0: Save setting LED_Update (indicate the state for the LED)
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+16, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;

Variable_Guardar=RunTime;
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+88, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}

.

.

.

 HAL_FLASH_Lock();
return 0;
}else{
return 1;
}
}

 

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Jan 25, 2025 10:54 AM UTC

For Emulating EEPROM in Flash on STM32F4, ST provide the STSW-STM32066 software pack, EEPROM emulation in STM32F40x/STM32F41x microcontrollers:

https://www.st.com/en/embedded-software/stsw-stm32066.html

See Application Note AN3969, EEPROM emulation in STM32F40x/STM32F41x microcontrollers for details:

https://www.st.com/en/embedded-software/stsw-stm32066.html#documentation

 

@Alejandra It may not exactly suit your requirements, but it does show how to use the STM32F4 Flash for data storage.

With that knowledge, you could adapt to your own needs; eg, see:
https://community.st.com/t5/stm32-mcus-embedded-software/eeprom-emulation-virtual-addresses/m-p/675964/highlight/true#M47888

and follow the link.

 

See also: https://community.st.com/t5/stm32-mcus-products/use-stm32f4-flash-for-non-volatile-data-storage-eeprom/m-p/743316/highlight/true#M266296

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

4 replies

TDK
Jan 24, 2025 9:07 PM UTC

Resetting the chip or removing power during a flash write operation can cause corrupted/incomplete data stored. That's most likely. Also possible is insufficient power for the chip, such as using operations that require 3.3V when you are only supply 2.7V.

"If you feel a post has answered your question, please click ""Accept as Solution""."
mbarg.1
Senior III
Jan 25, 2025 10:36 AM UTC

Aside all suggestions in @TDK post that I do totally agree, I would rise some more concerns.

Flash is NOT designed to be used as you are planning; tipically EEPROMS are the solution for incremental data storage.

But if you are unable to force hw design change, you must handle Flash as unreliable storage media.

This means using data buffering and performing readback checks for correct storage content before deleting data:

  • Save flash origina content somewhere;
  • Delete and write new data;
  • Read back flash;
  • Compare data with new data;
  • If data are correct, delete temporary stored data and move on;
  • Else retry delete and write new data;
  • Or restore original data.

Another concerns is relate to Flash lifecycle.

Check on datasheet if minimum number of cycles is enough for your application; do not allow products to go out and have some percentage of them undeperform.

Andrew Neil
Andrew NeilBest answer
Super User
Jan 25, 2025 10:54 AM UTC

For Emulating EEPROM in Flash on STM32F4, ST provide the STSW-STM32066 software pack, EEPROM emulation in STM32F40x/STM32F41x microcontrollers:

https://www.st.com/en/embedded-software/stsw-stm32066.html

See Application Note AN3969, EEPROM emulation in STM32F40x/STM32F41x microcontrollers for details:

https://www.st.com/en/embedded-software/stsw-stm32066.html#documentation

 

@Alejandra It may not exactly suit your requirements, but it does show how to use the STM32F4 Flash for data storage.

With that knowledge, you could adapt to your own needs; eg, see:
https://community.st.com/t5/stm32-mcus-embedded-software/eeprom-emulation-virtual-addresses/m-p/675964/highlight/true#M47888

and follow the link.

 

See also: https://community.st.com/t5/stm32-mcus-products/use-stm32f4-flash-for-non-volatile-data-storage-eeprom/m-p/743316/highlight/true#M266296

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.