Skip to main content
Associate III
March 14, 2024
Solved

Writing data to STM32G4 Flash

Sorry, my first time programming an STM32.  I have a bunch of data I need to store for a few hours, and the thought was to store it in Flash since there's a lot more of it (512k vs. 128k for regular RAM) but it looks to be pretty daunting. 

I've been reading a bunch of articles online, and they all seem to contradict each other, and they all say things like "all you do is write to the memory location, just like regular RAM" and then in the fine print it lists the 43 things you have to do first, - turn off IRQs, update control registers, etc., etc., etc.

Is there an example program for the STM32G474RE that shows a simple "write a bunch of data to Flash" and an equally simple "read a bunch of data from Flash"?

Thanks!

Chris

 

This topic has been closed for replies.
TDK
TDKBest answer
March 14, 2024

> Is there an example program for the STM32G474RE that shows a simple "write a bunch of data to Flash" and an equally simple "read a bunch of data from Flash"?

Here's one:

https://github.com/STMicroelectronics/STM32CubeG4/tree/master/Projects/NUCLEO-G474RE/Examples/FLASH/FLASH_EraseProgram

"If you feel a post has answered your question, please click ""Accept as Solution""."

5 replies

TDK
TDKBest answer
March 14, 2024

> Is there an example program for the STM32G474RE that shows a simple "write a bunch of data to Flash" and an equally simple "read a bunch of data from Flash"?

Here's one:

https://github.com/STMicroelectronics/STM32CubeG4/tree/master/Projects/NUCLEO-G474RE/Examples/FLASH/FLASH_EraseProgram

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate III
March 14, 2024

Brilliant, thank you!  If I'm reading the documentation right, the STM32 is in dual bank mode, am I allowed to read/write the Flash in bank 1 (where the program is) as long as I don't overwrite the program itself?

 

Associate III
March 14, 2024

And ... this code

uint32_t bank32address = 0x08040000;

uint64_t data = 0x12345678;

status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, bank32address, data);

status is HAL_ERROR