Skip to main content
Associate III
March 18, 2024
Solved

Write to Flash only 64Bit

Hello,

Can I only write to the flash with 64 bit variables, or also 32/16/8 bit?
I just used this function for this: HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, activepageaddress + u32_Offset, u64_Data)
I have an STM32L432 uC.

I already found this example: https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Projects/NUCLEO-L4P5ZG/Examples/FLASH/FLASH_FastProgram/Src/main.c

Many thanks in advance.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
March 18, 2024

Hello @Martin42 

Flash programming is only by 64-bits at a time. On other series it can be 32-bits.

STTwo32_0-1710763327109.png

For more details refer to this post.

Best Reagrds.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
March 18, 2024

Hello @Martin42 

Flash programming is only by 64-bits at a time. On other series it can be 32-bits.

STTwo32_0-1710763327109.png

For more details refer to this post.

Best Reagrds.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
March 18, 2024

You'd use a structure (packed?) or array to consolidate the smaller variables into a larger / usable block that fits the minimum write width of the FLASH memory. You'd then write as a block.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Martin42Author
Associate III
March 18, 2024

 

I would like to write a second firmware via Modbus and delete areas in the flash.
I send the raw HEX file using a PC tool and then write 64 bits at a time, since the flash only allows access with 64 bits.

To build the HEX file I use the addition "--gap-fill 0x00 --pad-to 0x08019000" to always get addresses with 32 bytes. This should also ensure that 64 bits are always written.
e.g. arm-atollic-eabi-objcopy.exe -O ihex --gap-fill 0x00 --pad-to 0x08019000 "${BuildArtifactFileBaseName}.elf" "${BuildArtifactFileBaseName}.hex"

-> Adds ":04018C00000000006F" the missing values for to fill 64 bit

 

:1001600059C0000859C0000859C00008000000002C
:1001700059C0000859C0000800000000000000003D
:0C01800059C0000859C0000859C0000810
:04018C00000000006F
:1001900010B5054C237833B9044B13B10448AFF3C1
:1001A00000800123237010BD1C010020000000000E

 

 

Tesla DeLorean
Guru
March 18, 2024

Not sure if there was a question there.

Either normalize the data on the host. Or as you process it on the target

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Martin42Author
Associate III
March 18, 2024

No question :)

I will do it on the target.