Skip to main content
Andreas S.
Associate II
October 5, 2017
Question

Write to flash in Early Wakeup Interrupt (EWI) of Window Watchdog (WWDG)

  • October 5, 2017
  • 0 replies
  • 543 views
Posted on October 05, 2017 at 15:48

Hi all,

I am working on a STM32F429 and I want to write some info to flash, e.g. the PC when the Window Watchdog triggers an reset. I have created a project in CubeMX and added the WindowWatchdog:

<code>

  hwwdg.Init.Prescaler = WWDG_PRESCALER_8;

  hwwdg.Init.Window = 127;

  hwwdg.Init.Counter = 127;

</code>

In EarlyWakeupInterrupt I refresh the watchdog and erase the sector 15 with VoltageRange 3 and write one byte to address 0x0810C000.

The EWI is triggered , but somehow it seems that the erase and write takes too long and the reset is triggered.

But when I add a timer (timer5) and capture the call to flash write it takes about 19000000 timer counts. With 90 MHz based timer count this is about 200 ms. Does this make sense? -> Yes, according to the DataSheet 6.3.13 Memory characteristics.

What would be a good way to store information about the system in case of an watchdog reset ?

Thanks and best regrads

Andreas

    This topic has been closed for replies.