Skip to main content
jf2399
Associate
June 15, 2009
Question

write DR on I2C1 cause Arbitration Lost Detected

  • June 15, 2009
  • 1 reply
  • 592 views
Posted on June 15, 2009 at 07:19

write DR on I2C1 cause Arbitration Lost Detected

    This topic has been closed for replies.

    1 reply

    jf2399
    jf2399Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:14

    Hi all,

    I'm trying to use the I2C1 on STM32F101, using the PB6 and PB7 pins.

    I have configure the pin, the register of I2C to place my STM32 in Master mode, no DMA and I can generate the Start bit on I2C bus.

    SB on SR1 change to 1 after the start, and when I Write slave device adress in DR, the chip tell me that there's an arbitration lost detected, and then Goes to Slave mode and free the bus.

    Have you and Idea about this problem ??

    Here's the init code and the test code .

    Init Code :

    Code:

    unsigned int tmp ;

    IC2CLOCKEN = 1; // a BBA to select clock on module I2C1

    I2C1REMAP = 0; // BBA on Remap port of I2C

    tmp= I2C->SR1 ;

    tmp= I2C->SR2 ;

    PE=1;

    I2C1->CR2 = 0x0002;

    I2C1->CCR = 0x0008;

    I2C1->TRISE = 5 ;

    PE=1;

    I2C1_SWRST = 1; // BBA for SWRST on CR1

    test code

    Code:

    unsigned int tmp ;

    I2C1_SWRST = 0;

    PE = 1 ;

    I2C_START =1; // BBA on START on CR1

    while (I2CSB !=1 ); // BBA on SB on SR1

    I2C1->DR = 0x64; // --->>> makes Arbitration Lost detected flag to 1