Question
Would like to use the UART on the STM32F429ZIT Discovery boart
Posted on April 04, 2014 at 03:22
I would like to use one of the UARTS on the STM32F4 to connect the MCU to a Bluetooth SMART controller. I was wondering if anyone could tell me if there is any access on the board to one of the UARTs so that i can solder wires to pull the RX/TX lines out. If so, which UART is it? I'm sure going through the schematic would tell me this, but I'm a noob to the really lowlevel embedded stuff and I've been looking at the schematic for a while and still can't figure it out. Any help would be much appreciated.
ThanksKartik #discovery #uart #stm32f4