Skip to main content
nj_boelskov
Associate III
June 10, 2008
Question

Works Ulink-me with STM3210B-EVAL?

  • June 10, 2008
  • 9 replies
  • 1668 views
Posted on June 10, 2008 at 07:37

Works Ulink-me with STM3210B-EVAL?

    This topic has been closed for replies.

    9 replies

    nj_boelskov
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Hi

    I just got a new kit (STM3210B-EVAL) to play with, but my ''old'' Ulink-me JTAG doesn´t seem to work with it. If I set the boot-switches to system memory, I can download to the uC, but I can not debug or execute the program. I cannot download if the switces are set to user flash?

    The kit came with a J-link JTAG from Segger, but do I need to use this? Need a License then :(

    -Niels

    nj_boelskov
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    ST has told me that the Ulink-me can not be used for the STM3210B-EVAL kit.

    Then you know it :)

    nj_boelskov
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Hi

    It came out, that it could be used anyway, but if it is used with the STM3210B-MCKIT, you cannot use the optical print, if you want to debug. Then you have to connect the ulink-me direct to EVAL-kit ;)

    cesar550v
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Quote:

    On 25-03-2008 at 09:19, Anonymous wrote:

    ST has told me that the Ulink-me can not be used for the STM3210B-EVAL kit.

    Then you know it :)

    Please can you tell me if Ulink-me is for a specific evaluation board. Or why you can not used it.

    Thanks

    cesar550v
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Quote:

    On 01-04-2008 at 08:28, Anonymous wrote:

    ULINK2 offers all the features of the original ULINK USB-JTAG Adapter plus 10MHz JTAG clock, RTCK support, Serial Wire Debug (SWD) support, Serial Wire Viewer (Trace) support, and a real-time agent.

    ULINK-ME is a reduced version of ULINK2 that only supports ARM-processor based devices using a 20-pin 0.1 inch connector.

    ULINK has been replaced by ULINK2.

    I dont know about the other microcontrollers, but I´m sure that you can connect to the stm32 using ULink-me

    Then I buy an Ulik Me because both are the same for ARM.

    thanks, very useful answer . :)

    nj_boelskov
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    ULINK2 offers all the features of the original ULINK USB-JTAG Adapter plus 10MHz JTAG clock, RTCK support, Serial Wire Debug (SWD) support, Serial Wire Viewer (Trace) support, and a real-time agent.

    ULINK-ME is a reduced version of ULINK2 that only supports ARM-processor based devices using a 20-pin 0.1 inch connector.

    ULINK has been replaced by ULINK2.

    I dont know about the other microcontrollers, but I´m sure that you can connect to the stm32 using ULink-me

    cesar550v
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Quote:

    On 31-03-2008 at 09:45, Anonymous wrote:

    Hi

    It came out, that it could be used anyway, but if it is used with the STM3210B-MCKIT, you cannot use the optical print, if you want to debug. Then you have to connect the ulink-me direct to EVAL-kit ;)

    Then I can buy one ulinkME for a LPC evaluation board and late I can connect to a STR750 ot STM32 without problems?

    What is the diference betwen ulink and ulink ME?

    Thanks

    :)

    [ This message was edited by: Tarlons on 31-03-2008 17:59 ]

    nj_boelskov
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    But Ulink-me can only be used with Keil uVision??

    and not if you e.g. are using the GCC compiler?

    [ This message was edited by: nj_boelskov on 10-06-2008 11:08 ]

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Hi All,

    ULink-ME is fully compatible with all STM32 boards and is the latest one from Keil/ARM in terms of features. In addition to its cheap costn, compact small size and you can power your board through its internal VDD ( 3.3volts) from your USB 5Volts.

    Cheers, STOne-32 :p