Skip to main content
russ
Associate III
Aug 10, 2009 11:58 AM UTC
Question

Wireless hopes and dreams

Posted on August 10, 2009 at 13:58

Wireless hopes and dreams

    This topic has been closed for replies.

    21 replies

    mkefalas
    Associate
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    Hi

    I'm quite experienced with radios short-long range and

    serial communications. If you are still looking for solutions

    contact me .

    russ
    russAuthor
    Associate III
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    I should note that there are numerous other IC's that I did research on and the ones in the spreadsheet are the most viable options I came across.

    russ
    russAuthor
    Associate III
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    Quote:

    On 29-01-2009 at 13:36, Anonymous wrote:

    Hi

    I'm quite experienced with radios short-long range and

    serial communications. If you are still looking for solutions

    contact me .

    I would love to get more recommendations for wireless. At this point I have done a good deal of research on this subject and my conclusion is that the Nordic nRF24LE1 is our best option. It has a great price point and good reference designs. I have included my analysis in a spreadsheet which may be helpful to others on my same path. It has prices, including developement costs, and IDE tool costs.

    mkefalas
    Associate
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    Ok Russ1

    I will give you some directions since the subject of RF and transmission

    requires a lot of expertise and some consider it ''black art''.

    Separate first of all two worlds and one is the radio part

    and the second is the digital part .

    It's funny to evaluate radios in terms of standby current and data rate

    since for radio guys the real parameters judging the reliability of a radio

    are usually hidden or specified very shortly.

    Keys parameters in a radio design regarding the receiver are it's noise figure , compression point, image rejection, adjacent channel rejection and a long list of other parameters that mainly describe the range you will achieve and the behaviour your link will have if it's surrounded by other closely operating rf links .

    Regarding the transmitter you have parameters such as output power , adjacent channel leakage , modulation efficiency , harmonics suppresion etc. Finally the antenna is another serious factor not to be taken lightly as is the path loss calculation, fading etc.

    These chipsets you are referring on the market are not designed for anything serious regarding radio performance.

    For example it's nice to see those +10 dbm chipsets operating at 2.4 GHZ but it's doudtfull the results you will achieve operating in frequencies occupied with other wlan's . Don't expect a long range link . On the other side if your demands are short range then you can give it a try.

    Follow these rules

    Use a formula to calculate open space path loss so you evaluate ''link budget'' offered by the chipset.

    If you see high sensitivity in a chipset check immediately compression of the receiver.

    If you need extra db's power check antenna alternatives .

    Adding an amplifier will add up to a mess that usually leads to trouble since these chipsets are not easy to deal (extra isolation etc.) Finally legal problems if you transmit higher than power dictated by regulations and if you don't have a spectrum analyzer handy usually spurious and harmonics are the rule.

    IN the past i have designed for a customer short range in house wireless link based on the nRF2401 .Speed i have achieved is 57600 bps and it was working with an AVR . No protocol is required since it was just a virtual serial port. What nRF2401 lacks is RSSI , easy amplifier connection , and the receiver is not of serious performance (as most of these chipsets anyway) . The specs though regarding distance and cosumption were ok so i implemented it .You don't need a protocol to implement what you want .Code size was about 2K written with a c compiler . What the nRF2401 is missing is an RSSI measurement and easy external amplifier connection (the rx-tx switch is inside) .Although the link budget was marginal i implemented prototype based feed closed dipole antenna printed on FR4 that gave omnidirectional coverage and added another 2.1 dBi (If you don't have a vector network analyzer then you need black art !!! to tune it) that increased the link performance to acceptable values.

    From my research recently, i like the CC1101 with STM32Fxx which seems more adequate for long range communications (with external modifications) and low power consumption but if you don't test these things by yourself you can't easily express an opinion .

    Sorry for my long talk but it's a big subject.!!!

    [ This message was edited by: mkefalas on 29-01-2009 20:23 ]

    russ
    russAuthor
    Associate III
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    I wasn't aware of that. Thank you.

    m3allem
    Associate
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    Hi russ1;

    I saw your sheet and you sayed that Must write stack and protocol in the case of STM32, but I think that OLIMEX has write the driver of nRF24L04 with stm32.

    I attach the driver.

    PS: the driver is available on www.olimex.com

    B.R.

    M3allem

    tomas239955
    Visitor II
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    Check out www.connectblue.com for a wide range of Bluetooth serial port adapter modules.

    /Tomas

    mkefalas
    Associate
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    Dear Russ1

    Nordic will give you +7-8 dBm output power .

    Now you have to design your link at -60 dBm.

    Where you are loosing is the fact that nordic

    needs 1MHZ BW since its designed for 1 mbit

    communication so that dictates low sensitivity

    since you need a lot of BW .If you use narrow BW

    (25 KHZ is sufficient for 9.6 kBps)

    communication you increase sensitivity and operate reliably

    at -90 dBm .To give you the idea every 6 dB you double the

    distance so from -60 to -90 dbm you have 2x2x2x2x2=32 times

    nRF24L01 distance.

    Use Riis formula to calculate path loss you need to cover at that frequency and start your calculations.

    In 1997 i designed a link at 2MBps @2.0 GHZ with a range of 30 km. Like the ones that drive parabolic antennas the one you see in Telecoms towers.

    That is long range

    Short range are +10 dBm output devices.

    I don't want to fire a conversation about these terms since a 10 dBm device can go 50 km but it's just the feeling i want to give you .

    The CC1101 doesn't require an amplifier for 100-130 feet L.O.S .Just don't neglect a good antenna . You can also use nRF2401 without amplifier but forget these things you see in printed antennas included in application manuals.

    Wish you the best with your design

    russ
    russAuthor
    Associate III
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    mkefalas,

    Thank you very much for your insights. I guess it takes an expert on the subject to teach me how little I know. I really appreciate it. Back to researching I go. Can you recommend any other resources on this subject. You mentioned modulation efficiency and RSSI; I am going to need to look up more details about such critical RF design points.

    You also mentioned short and long range communication. My question is how you are defining the two terms. My goal is a very strong RF link (in the 2.4GHz band) over 100-130 feet (line of sight). Is this doable with the Nordic parts? Also, I am not going to be using an amplifier.

    [ This message was edited by: russ1 on 29-01-2009 20:48 ]

    fenice1953
    Visitor II
    May 17, 2011 10:45 AM UTC
    Posted on May 17, 2011 at 12:45

    Hi all,

    congratulation for all the information you wrote! I'm a new user and I'd like to ask you an information. I'm totally new in this field thus I hope to avoid silly questions!

    I have a SAM9L9260 board, with ARM9 micro on board. So far, I connect the Ethernet port to a D-link device able to enabling a wireless connection.

    My question is: is it possible to skip the Ethernet port adding a wireless chip-set? should I consider both chip-set and tranceiver.. ?

    Any advise??

    thanks