Skip to main content
ACALI.1
Visitor II
April 25, 2022
Question

Will using APM 32 MCUs produced and sold by GEELY company instead of STM32 cause any license violation? The code I compiled for ST works in APM32.

Will using APM 32 MCUs produced and sold by GEELY company instead of STM32 cause any license violation?

    This topic has been closed for replies.

    10 replies

    Peter BENSCH
    ST Technical Moderator
    April 25, 2022

    Welcome, @ACALI.1​, to the community!

    None of the clones were licensed by STMicroelectronics to any other manufacturer. It does not matter that the software on these clones may work in the same way. Yes, in this respect you are violating the licence conditions that are mentioned for the Firmware libraries in their Software Package License Agreement SLA0048 (the following is an excerpt):

    2. Redistributions in binary form, except as embedded into microcontroller or microprocessor device manufactured by or for STMicroelectronics or a software update for such device, must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

    [...]

    4. This software package or any part thereof, including modifications and/or derivative works of this software package, must be used and execute solely and exclusively on or in combination with a microcontroller or a microprocessor devices manufactured by or for STMicroelectronics.

    By the way, it is also mean and disrespectful of the manufacturer's work to use their freely provided software to use it on cheap clones.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Piranha
    Principal III
    April 27, 2022

    Ironically, except for SBSFU and probably few other packages, ST's own attitude to thw quality of ST's firmware code for STM32 microcontrollers is on the same level of disrespect against customers, who are supposed to use it.

    Peter BENSCH
    ST Technical Moderator
    April 27, 2022

    @Piranha​ Free software and firmware is disrespectful to customers?

    Isn't that a tiny bit harsh?

    You are very welcome to contribute with improvements to the firmware via the Github repository.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Tesla DeLorean
    Guru
    April 25, 2022

    You might also want to check that GEELY has paid all patent pool and IP licencing appropriately, and that your products don't violate other IP holders rights.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Piranha
    Principal III
    April 27, 2022

    To read the licence text, one has to learn the spelling. Geely is a car maker.

    Visitor II
    June 16, 2024

    think that employee at st need to realised that seggers partner with amp , so it doesnt look like a violation and seems like geehy payed their full diligence

     

     

    https://www.segger.com/news/segger-and-geehy-partner-to-fully-support-the-apm32-series-mcu/

     

    Peter BENSCH
    ST Technical Moderator
    June 16, 2024

    @cutterhead Please read the text on the website again - it only states that Segger also supports those MCUs with its J-LINK. This has NOTHING to do with an agreement between that manufacturer and STMicroelectronics regarding the MCUs.

    The use of software and/or libraries from STMicroelectronics without such an agreement - which, by the way, can only be made with STMicroelectronics - is clearly a violation of the above-mentioned licence conditions.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.