Skip to main content
VaZso
Associate III
September 29, 2022
Solved

Will software of STM32F407ZET6 work in STM32F407ZGT6?

Dear Community,

I would like to request manufacturing additional board for a project but currently PCB assembling partner doesn't have STM32F407ZET6 in stock but it has STM32F407ZGT6.

Basically, these two MCUs have the same capabilities except ZGT6 has double amount of flash memory which I don't need to use.

Should I afraid loading the same software in ZGT6 would cause problems?

So I would only use 512kB of flash but I would like to download the same firmware.

It is because I have an own boot loader and remote upgrade possibility and I would not like to handle two separate chips for remote upgrade because of the inability to source the very same chip.

Theoretically they should not have more difference other than their flash size.

Do anyone have any experiences or ideas?

Also, would development environment (STM32CUBEIDE) allow programming a ZET6 project into a ZGT6 chip?

Thank you your help in advance.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
September 30, 2022

Same Die, More Flash Tested, Spent more time on tester.

Time has a direct relationship to throughput on the line, and thus cost.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
September 30, 2022

Same Die, More Flash Tested, Spent more time on tester.

Time has a direct relationship to throughput on the line, and thus cost.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
VaZso
VaZsoAuthor
Associate III
September 30, 2022

Thanks.

I thought the same but I would like to be sure and I am also afraid IDE may complain (which it should not as only the flash is bigger).

The alternative is to source the original chip elsewhere then do a hand-soldering which I would like to avoid doing for several boards...

So I really hope picking the bigger version will mot mess up anything.