Skip to main content
Clament John
Associate II
Apr 21, 2017 10:13 AM UTC
Solved

Will an OFF state STM32 power up during SPI transaction

Posted on April 21, 2017 at 12:13

We know a micro can be powered up using its GPIO. If you didn't know - 

https://www.eevblog.com/forum/blog/eevblog-831-power-a-micro-with-no-power-pin!/

I have an STM32F0103 which will be in OFF state (VCC = 0 V) and another uC which will be connected to it through SPI. The second uC can initiate an SPI transaction - call chip select, send SCK etc, but the STM is still in its OFF state. So my question is

1.Will this cause the STM to get powered for a brief duration (when the pin is high)? I know it won't get enough current (the second uC GPIO pin won't supply enough), but will this flickering power cycle cause problems?

2.What should I do to prevent this if it happens?

#power-management #stm32
    This topic has been closed for replies.
    S.Ma
    S.MaBest answer
    Principal
    Apr 21, 2017 6:57 PM UTC
    Posted on April 21, 2017 at 20:57

    The application implementation seems risky reliability speaking.

    The unpowered GPIOs might degrade the transiting SPI device signals.

    True open dain 'power fail safe' SDA/SCL pins of an I2C bus mode would be better suited at lower bitrate.

    Otherwise maybe adding cheap serial resistors on the SPI lines going to the unpowered SPI device to minimize issues?

    1 reply

    S.Ma
    S.MaBest answer
    Principal
    Apr 21, 2017 6:57 PM UTC
    Posted on April 21, 2017 at 20:57

    The application implementation seems risky reliability speaking.

    The unpowered GPIOs might degrade the transiting SPI device signals.

    True open dain 'power fail safe' SDA/SCL pins of an I2C bus mode would be better suited at lower bitrate.

    Otherwise maybe adding cheap serial resistors on the SPI lines going to the unpowered SPI device to minimize issues?