Skip to main content
Visitor II
December 15, 2023
Question

WiFi Firmware for B-L4S5I-IOT01A

  • December 15, 2023
  • 2 replies
  • 1340 views

Hi,

I am facing a problem to connect the B-L4S5I-IOT01A STM32 board to Wifi. I downloaded X-Cube-AWS.

And STM32L4 Discovery Kit IoT Node (B-L475E-IOT01A) ISM43362-M3G-L44-SPI-C3.5.2.7.STM SPI Firmware but still fails to connect.

Please if anyone can provide the steps to connect the wifi module to the mentioned board.

Greetings

Mrinalini

2 replies

ST Technical Moderator
December 17, 2023

Hello @mrinalinibarik,

You can have a look at the WiFi examples of communication between the STM32L4S5 and ISM433 WiFI chips with SPI by looking at STM32Cube L4 FW package in /Projects/B-L4S5I-IOT01/applications/WiFi (Common/Src/Wifi.c and es_wifi.c)

Hope this helped you!

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Guillaume K
ST Employee
January 26, 2024

Hello

What WiFi access point are you using ?

Are you using an iPhone or iPad as access point ? If yes, recent versions of iOS use WPA3 for WiFi security and B-L4S5I-IOT01A WiFi module doesn't support it.