Skip to main content
DK.7
Associate III
August 3, 2021
Question

Why the led 'PA1' turns on after switching 'on' a register "*GPIOA_MODER" and turns 'off' after the switching 'on' a register "*GPIOA_ODR"?

  • August 3, 2021
  • 5 replies
  • 877 views

I'm studying a registers...

I have stm32407vg and the LED is on the 'PA1' and I need that the LED turned 'On' after command witch It should turn it 'ON'. In may case after line № 18.

But 'LED' turns 'ON' after line №16 and turns 'OFF' after line № 18

Could you tell me why it happens?

Below my code.

#include <stdint.h>
/*
#if !defined(__SOFT_FP__) && defined(__ARM_FP)
 #warning "FPU is not initialized, but the project is compiling for an FPU. Please initialize the FPU before use."
#endif
*/
int main(void)
{
	uint32_t *RCC_AHB1ENR = (uint32_t*)0x40023830; // Base address + Adress ofset=0x30 from table "RCC AHB1 peripheral clock register (RCC_AHB1ENR)"
	uint32_t *GPIOA_MODER = (uint32_t*)0x40020000;// Base address + Adress ofset=0x00 from table "GPIO port mode register (GPIOx_MODER) (x = A..I/J/K)"
	uint32_t *GPIOA_ODR = (uint32_t*)0x40020014;// Base address + Adress ofset=0x14 from table "GPIO port output data register (GPIOx_ODR) (x = A..I/J/K)"
 
	// 1. Enable the clock for GPIOA peripheral in the AHB1ENR
	*RCC_AHB1ENR |= 1<<0; 
	// 2. Configure the mode of the IO pin a output
	*GPIOA_MODER |= 0<<3 | 1<<2; 
	// 3. SET 1th bit of the uotput data register to make I/O pin-1 a HIGH
	*GPIOA_ODR |= 1<<1; 
	/* Loop forever */
	while(1){
	 // for(uint32_t i=0; i < 300000; i++ );
	 // *GPIOA_ODR |= 1<<0;
	 // for(uint32_t i=0; i < 300000; i++ );
	 //*GPIOA_ODR &= ~(1<<0);
	 }
}

This topic has been closed for replies.

5 replies

waclawek.jan
Super User
August 3, 2021

Is the LED connected cathode to PA1 and anode through resistor to VCC?

JW

DK.7
DK.7Author
Associate III
August 3, 2021

How can I find out it?

Here is a link to my stm32f407vg https://stm32-base.org/boards/STM32F407VGT6-STM32F4XX-M.html#User-LED

TDK
August 3, 2021

You should use the CMSIS header files rather than recreating your own. It will make your program more readable and avoid mistakes.

One mistake here is that you do not quality the address as volatile, which means the compiler is allowed to optimize out the access if there are no other consequences.

PA1 needs to be low in order to turn on the LED.

0693W00000D1PJWQA3.png

"If you feel a post has answered your question, please click ""Accept as Solution""."
DK.7
DK.7Author
Associate III
August 3, 2021

Thank you answer! Of course I will use the CMSIS header files...

Question about "volatile" Is it correct in my case?

uint32_t *RCC_AHB1ENR = (*(volatile*)0x40023830);

TDK
August 3, 2021

No.

volatile uint32_t * RCC_AHB1ENR = (volatile uint32_t *) 0x40023830;

Just use the header files instead.

"If you feel a post has answered your question, please click ""Accept as Solution""."