Skip to main content
majd-ghadab
Associate II
November 20, 2021
Question

Why SDRAM1 and SDRAM2 have the same pins

  • November 20, 2021
  • 3 replies
  • 1116 views

Hello,

can someone please help me,

why do when i use SDRAM1 and then add SDRAM2 the data and address pins are the same but only the chip enalbe. does this mean that all pins even the Data pins DQ can be connected parallel for both chips? have someone a reference design that uses both SDRAM controllers in the same time. Thanks in advance.

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    November 21, 2021

    That's why you have chip selects, otherwise they'd use too many pins.

    Perhaps you need a HW Design Engineer on your team?

    https://community.st.com/s/question/0D50X0000BNtpmlSQB/parallel-sdram

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    majd-ghadab
    Associate II
    November 21, 2021

    Hello Tesla, thank you again for the support.

    Please one more thing, so should i use 2 times 22Ohm resistors for the same pin from each sdram then connect them to MCU or one 22Ohm resistor is enough so the node will go to bothe sdrams?

    for your question about the HW Design Engineer, it not easy to get everything when you are at the beginning.

    TDK
    November 21, 2021

    Inline resistors are there for signal integrity, which will be dependent on your specific layout and environment. Generally, if the traces are short, you don't need inline resistors on data lines.

    "If you feel a post has answered your question, please click ""Accept as Solution""."