Skip to main content
NRatz.2
Associate II
August 25, 2022
Question

Why is my HAL_CAN_RxFifo0MsgPendingCallback function not getting called?

  • August 25, 2022
  • 1 reply
  • 878 views

I'm new to the STM32Cube series, and I'm using the STM32Cube MX L4 chipset. I believe I've done everything that online tutorials, examples, and the actual specs demand, but when my code issues HAL_CAN_AddTxMessage, my ISR never gets called. What am I missing?

Here's my code:

/* USER CODE BEGIN 0 */
// TODO: programmatically retrieve the actual CAN ID
#define NOJI_DEFAULT_ID 102
uint8_t currentID = NOJI_DEFAULT_ID;
CAN_TxHeaderTypeDef txHeader;
CAN_RxHeaderTypeDef rxHeader;
uint8_t txData[8];
uint8_t rxData[8];
uint32_t txMailbox;
int dataCheck = 0;
 
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *Nhcan)
{
	static uint32_t count = 0;
	count++;
	memset((void *) &rxHeader, 0, sizeof(CAN_RxHeaderTypeDef));
	memset((void *) rxData, 0, 8);
	HAL_CAN_GetRxMessage(Nhcan, CAN_RX_FIFO0, &rxHeader, rxData);
	if (rxHeader.DLC == 1)
	{
		dataCheck = 1;
	}
}
HAL_StatusTypeDef Noji_CAN_Start(CAN_HandleTypeDef *Nhcan)
{
	HAL_StatusTypeDef status = HAL_OK;
	CAN_FilterTypeDef canFilter;
	memset((void *) &canFilter, 0, sizeof(CAN_FilterTypeDef));
	canFilter.FilterActivation = CAN_FILTER_ENABLE;
	canFilter.FilterBank = 4;
	canFilter.FilterFIFOAssignment = CAN_RX_FIFO0;
	canFilter.FilterIdHigh = currentID << 5;
	canFilter.FilterMaskIdHigh = currentID << 5;
	canFilter.FilterMode = CAN_FILTERMODE_IDMASK;
	canFilter.FilterScale = CAN_FILTERSCALE_32BIT;
	canFilter.SlaveStartFilterBank = 10;
	status = HAL_CAN_ConfigFilter(Nhcan, &canFilter);
	status = HAL_CAN_Start(Nhcan);
	status = HAL_CAN_ActivateNotification(Nhcan, CAN_IT_RX_FIFO0_MSG_PENDING);
	memset((void *) &txHeader, 0, sizeof(CAN_TxHeaderTypeDef));
	txHeader.IDE = CAN_ID_STD;
	txHeader.RTR = CAN_RTR_DATA;
	txHeader.StdId = currentID;	// 0x66
	txHeader.DLC = 1;
	txHeader.TransmitGlobalTime = DISABLE;
	memset((void *) txData, 0, 8);
	txData[0] = 0xD7;
	status = HAL_CAN_AddTxMessage(Nhcan, &txHeader, txData, &txMailbox);
	return status;
}
/* USER CODE END 0 */

and then Noji_CAN_Start is called from MX_CAN1_Init immediately after the call to HAL_CAN_Init

Thanks!

This topic has been closed for replies.

1 reply

NRatz.2
NRatz.2Author
Associate II
August 31, 2022

Ok, no answer. Well, let's try a different approach. What can I do in the STM32 firmware to advertise my ID / presence on the CAN bus? Using DroneCAN, I can't see my device, possibly because it doesn't register / advertise its ID on the bus. Thoughts?