Why is my current comsumption much higher in standby than what is mentionned in the Datasheets
Hello guys,
I've been trying to enter the Standby Mode using the Exemples from st and i got it work. But in Standby i'm still around 6mA.
This is much more than the expected 5 µA! Maybe someone knows what may cause this Behaviour?
thank you for your help!
/*My Code*/
#define PWR_WAKEUP_PIN_FLAGS (PWR_WAKEUP_FLAG1 | PWR_WAKEUP_FLAG2 | PWR_WAKEUP_FLAG3 | PWR_WAKEUP_FLAG4 | PWR_WAKEUP_FLAG5 | WR_WAKEUP_FLAG6)
void vtest2(void* Param)
{
/* Check and handle if the system was resumed from StandBy mode */
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
/* Clear Standby flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB_D1);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB_D2);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_PIN_FLAGS);
}
/*Disablke WakeUp Pin*/
HAL_PWREx_DisableWakeUpPin(PWR_WAKEUP_PIN4);
/* Clear all related wakeup flags */
HAL_PWREx_ClearWakeupFlag(PWR_WAKEUP_FLAG4);
PWREx_WakeupPinTypeDef sPinParams;
/* Enable WakeUp Pin PWR_WAKEUP_PIN4 connected to PC13*/
sPinParams.WakeUpPin = PWR_WAKEUP_PIN4;
sPinParams.PinPolarity = PWR_PIN_POLARITY_HIGH;
sPinParams.PinPull = PWR_PIN_NO_PULL;
HAL_PWREx_EnableWakeUpPin(&sPinParams);
/*Enter Standby*/
HAL_PWREx_EnterSTANDBYMode(PWR_D1_DOMAIN);
HAL_PWREx_EnterSTANDBYMode(PWR_D2_DOMAIN);
HAL_PWREx_EnterSTANDBYMode(PWR_D3_DOMAIN);
HAL_PWREx_ConfigD3Domain(PWR_D3_DOMAIN_STOP);
HAL_RCC_DeInit();
HAL_PWR_EnterSTANDBYMode();
while_(1)
{
}
}