Skip to main content
antonius
Associate III
October 7, 2013
Question

Why is my code sometimes running sometimes not ?

  • October 7, 2013
  • 14 replies
  • 1968 views
Posted on October 08, 2013 at 01:50

Guys,

Why is my code sometimes running sometimes not ?

When I plug in J-Link, it's stable but if I plug it out, it's not stable ??

Is it because a power supply from USB ?

Any ideas ?

Thanks
    This topic has been closed for replies.

    14 replies

    Tesla DeLorean
    Guru
    October 8, 2013
    Posted on October 08, 2013 at 02:36

    The universe of problems is pretty large, I could get my magic eight ball out?

    If you think it's a supply issue, then use a bench supply, and observe current draw.

    Track down what happens when the debugger is not attached, output diagnostic information via a serial port, or identify progress with GPIO or LED. Make sure you have a Hard Fault handler that can output data about faults.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    antonius
    antoniusAuthor
    Associate III
    October 8, 2013
    Posted on October 08, 2013 at 13:01

    or because I left my boot 1 hanging ?

    I boot from flash...

    antonius
    antoniusAuthor
    Associate III
    October 8, 2013
    Posted on October 08, 2013 at 13:03

    with LED blinker test it's stable, I'm using 2.4'' LCD, could it be the cause ? I have less power to turn it on ?

    Now it's on after trying to reset few times....

    frankmeyer9
    Associate III
    October 8, 2013
    Posted on October 08, 2013 at 17:15

    Power consumption can be a problem with LCD displays. Supplying by USB might not be sufficient, as I can confirm. But that should be easy to find out.

    LCD displays need relatively long delays at startup, to ramp up internal voltage converters - up into hundreds of milliseconds. Check the datasheet of your display. They usually provide an example initialization sequence, which you can compare with your code.

    jj2
    Associate
    October 8, 2013
    Posted on October 08, 2013 at 23:36

    Appreciate all advice thus far - but perhaps this, ''When I plug in J-Link, it's stable but if I plug it out, it's not stable'' deserves further regard?

    If that probe attachment improves things - as you state - might that suggest inadequate Reset circuit handling and/or JTAG pins not properly, ''pulled-up?''  Thus - w/JTAG probe present - those connections/signals are rendered ''proper'' - and when absent - improper connections assert... 

    To remove ''inadequate power'' from the mix - suggest that you open the connection to Lcd's backlight - likely the biggest power-hog on your board - and see if issue resolves...
    antonius
    antoniusAuthor
    Associate III
    October 8, 2013
    Posted on October 09, 2013 at 01:43

    I put 10uF capacitor on VDD3,as suggested on datasheet and I call it stable now, not sure....but everytime startup, I must push reset button few seconds to make it on...I'm using external power supply now

    The first time I applied power supply, LCD was off, I need to push reset button about 1 second to make it on, any ideas why ?

    Please have a look on my reset and JTAG circuit, in case I need a fix on it, thanks

    ________________

    Attachments :

    STM32F103V.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I07u&d=%2Fa%2F0X0000000baT%2FdXSDV2fn9ZU.1ZLAaJRHwN_QoR1Rqe9FnQc8jd_FdX4&asPdf=false
    antonius
    antoniusAuthor
    Associate III
    October 15, 2013
    Posted on October 16, 2013 at 00:32

    If I'm using USB as power supply, it's not easy to on it, even I push reset button so long..

    but if I'm using 1A transformer, I can make it start after pushing the reset button for a few seconds, is it because of the LCD consuming a lot of power ? I'm using 2.4'' LCD with ILI9325 controller...

    thanks

    antonius
    antoniusAuthor
    Associate III
    October 15, 2013
    Posted on October 16, 2013 at 00:48

    I'm gonna use Amp meter to see the current draw.....and get back to you guys...

    It's 132 mA on 5V input, I'm using 1A transformer and LCD backlight is on, I need to push reset button for few seconds to make it on and stable.....any ideas why ?

    thanks for the suggestion

    jj2
    Associate
    October 16, 2013
    Posted on October 16, 2013 at 22:37

    Your first post stated, ''When I plug in J-Link, it's stable but if I plug it out, it's not stable ??''

    Does this, ''JLink connection'' continue in making things stable?  (appears it does not - from the bulk of your follow-on writings)

    As others have stated - LCD Controllers - upon power-up - often require an unusually long time to become, ''Ready.''  Does your MCU Reset process also reset the LCD Controller?  If it does not - that added ''MCU-only'' Reset may provide the added time required by your LCD...

    Many LCD Controllers may ''signal'' their ''readiness'' to accept initialization & data.  Your compliance w/this is an ideal means to gain stable & repeatable LCD operation...

    antonius
    antoniusAuthor
    Associate III
    October 18, 2013
    Posted on October 18, 2013 at 08:41

    the solution I have now, is push the reset button for few seconds even until almost 10 seconds to make it on....

    From no power ==> power supply connected, LCD is blank forever if I'm not pushing the reset button....

    Is it because of reset circuit ?

    I'm not using J-Link anymore now, it's only LCD, STM32 and power supply...