why i get the VDDA value from VREFINT is wrong ?
I use MCU STM32L073, set VDDA=VREF+=3.29V, VSSA=VREF-=GND=0V.
I read Vrefint_cal for (0x1FF80078), get the value of Vrefint_cal = 0x680
get Vrefint_data from ADC_CHANNEL_17, get this value is Vrefint_data =0xbb7
the code is here:
////////////////////////////////////////////////////////////
HAL_ADCEx_EnableVREFINT();
sConfig.Channel = ADC_CHANNEL_17;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
//open adc
if (HAL_ADC_Start(&hadc) != HAL_OK)
{
Error_Handler();
}
HAL_ADC_PollForConversion(&hadc, 100);
if ((HAL_ADC_GetState(&hadc) & HAL_ADC_STATE_REG_EOC) == HAL_ADC_STATE_REG_EOC)
{
/* Get the converted value */
Vrefint_data = HAL_ADC_GetValue(&hadc);
}
Vrefint_cal=*(__IO uint32_t*)(0x1FF80078);
Vdda=3.3*(Vrefint_cal)/Vrefint_data;
printf("Vrefint_cal=%#x,Vrefint_data=%#x Vdda=%#f\r\n",Vrefint_cal,Vrefint_data,Vdda);
//////////////////////////////////////////////////////////
use Vdda=3.3*(Vrefint_cal)/Vrefint_data; I cout vdda = 1.831010, not 3.9V , why???