Question
Why I cannot read SPI via HAL but can directly through registers?
I am using stmf413xx to talk to M25P16 via SPI. I have working code that can send and receive data to flash via SPI but when I transition to HAL (I want get to interrupts eventually) it no longer works.
The code that works is
while ((SPI3->SR & SPI_FLAG_TXE) == 0) {}
volatile uint32_t tmp;
tmp = SPI3->DR; // to clear RXNE
(void)tmp;
SPI3->DR = byte;
while ((SPI3->SR & SPI_FLAG_RXNE) == 0) {}
return SPI3->DR;The code that does not work is
if(HAL_SPI_Transmit(spi_handle, &byte, 1, 1000) != HAL_OK)
{
log("failed 72");
}
if(HAL_SPI_Receive(spi_handle, &byte, 1, 1000))
{
log("failed 76");
}Both HAL_SPI_Transmit and HAL_SPI_Receive are successfull.
My SPI config is
SPI_HandleTypeDef hal_handle =
{
.Instance = SPI3,
.Init =
{
.Mode = SPI_MODE_MASTER,
.Direction = SPI_DIRECTION_2LINES,
.DataSize = SPI_DATASIZE_8BIT,
.CLKPolarity = SPI_POLARITY_HIGH,
.CLKPhase = SPI_PHASE_2EDGE,
.NSS = SPI_NSS_HARD_OUTPUT,
.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2,
.FirstBit = SPI_FIRSTBIT_MSB,
.TIMode = SPI_TIMODE_DISABLE,
.CRCCalculation = SPI_CRCCALCULATION_DISABLE,
.CRCPolynomial = 10
}
};
SPI_HandleTypeDef * spi_handle = &hal_handle;SPI_HandleTypeDef * spi_handle = &hal_handle;