Why I am stuck in I2C_ISR_TXIS flag set?
I have MPU6050 accerlometer, i need to interface with stm32f0 (via I2C).
Firstly i am check if the sensor is responding by reading the
"WHO_AM_I (0x75)" Register.
If the sensor responds with 0x68, this means it’s available and good to go.
but the code is stuck in while(I2C_GetFlagStatus(I2C1, I2C_ISR_TXIS) == RESET){} ,
why this happens?
__inline static void stm32_I2cSetup(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
I2C_InitTypeDef I2C_InitStructure;
#if _I2C1_ENABLE__
/* Configure the I2C clock source. The clock is derived from the HSI */
RCC_I2CCLKConfig(RCC_I2C1CLK_HSI);
/* I2C_SCL_GPIO_CLK and I2C_SDA_GPIO_CLK Periph clock enable */
RCC_AHBPeriphClockCmd(I2C1_SCL_GPIO_CLK | I2C1_SDA_GPIO_CLK, ENABLE);
/* I2C Periph clock enable */
RCC_APB1PeriphClockCmd(I2C1_CLK, ENABLE);
/* Connect PXx to I2C_SCL*/
GPIO_PinAFConfig(I2C1_SCL_GPIO_PORT, I2C1_SCL_SOURCE, I2C1_SCL_AF);
/* Connect PXx to I2C_SDA*/
GPIO_PinAFConfig(I2C1_SDA_GPIO_PORT, I2C1_SDA_SOURCE, I2C1_SDA_AF);
/* GPIO configuration */
/* Configure I2C pins: SCL */
GPIO_InitStructure.GPIO_Pin = I2C1_SCL_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(I2C1_SCL_GPIO_PORT, &GPIO_InitStructure);
/* Configure I2C pins: SDA */
GPIO_InitStructure.GPIO_Pin = I2C1_SDA_PIN;
GPIO_Init(I2C1_SDA_GPIO_PORT, &GPIO_InitStructure);
/* I2C configuration */
/* sEE_I2C configuration */
I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;
I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable;
I2C_InitStructure.I2C_DigitalFilter = 0x00;
I2C_InitStructure.I2C_OwnAddress1 = 0x00;
I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;
I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
I2C_InitStructure.I2C_Timing = I2C1_TIMING;
/* Apply sEE_I2C configuration after enabling it */
I2C_Init(I2C1, &I2C_InitStructure);
/* sEE_I2C Peripheral Enable */
I2C_Cmd(I2C1, ENABLE);
// /* Select the EEPROM address */
// SlaveAddr = 0x60;
Current_I2C = I2C1;
#endif
#if _I2C2_ENABLE__
#endif
}
void reg_read(void)
{
uint32_t Data = 0;
while(I2C_GetFlagStatus(I2C1, I2C_ISR_BUSY) != RESET){;;}
I2C_TransferHandling(I2C1,0x68, 1, I2C_Reload_Mode, I2C_Generate_Start_Write); //I2C_SoftEnd_Mode
while(I2C_GetFlagStatus(I2C1, I2C_ISR_TXIS) == RESET){}
I2C_SendData(I2C1,0x75);
while(I2C_GetFlagStatus(I2C1, I2C_ISR_TC) == RESET){}
I2C_TransferHandling(I2C1, 0x68, 1, I2C_AutoEnd_Mode,I2C_Generate_Start_Read);
while(I2C_GetFlagStatus(I2C1, I2C_ISR_RXNE) == RESET) { }
Data= I2C_ReceiveData(I2C1);
while(I2C_GetFlagStatus(I2C1, I2C_ISR_STOPF) == RESET) {}
I2C_ClearFlag(I2C1, I2C_ICR_STOPCF);
memset(ucGBuff1,0,sizeof(ucGBuff1));
sprintf((char *)ucGBuff1,"C: %d",Data);
printk((char *)ucGBuff1);
}
void printk( char* string)
{
u32 len = strlen(string);
USART_SendData(USART1,(u8 *)string,len);
}