Question
Why does STM32Cube recommend to not use SysTick
Posted on June 27, 2018 at 22:08
as TimeBase Source?
Today, I've been trying to activate FreeRTOS' USE_TICKLESS_IDLE feature.
It turns out that the tickless idle --in fact it is a unnecessary tick suppression-- works only when Timebase Source is SysTick because it is hard-coded so in the FreeRTOS port. (I'm using the latest CubeMX and firmware package.)
While this is perfectly fine for me, I'm curious why CubeMX keeps recommending not tu use SysTick as Time Base.
Thanks, Phil
#tickless-idle #systick #stm32l476rg