Skip to main content
JohnFrancis
Associate III
May 7, 2025 10:11 AM UTC
Solved

Who Sets the BFB2 Bit After Option Bytes Erase in STM32G4?

Hello, I am working with an STM32G4 microcontroller and noticed an unexpected behavior regarding Bit 20 (BFB2) in the User & Read Protection Option Bytes.

  • According to the reference manual, BFB2 is a read-only bit.

  • After performing an option bytes erase in Keil, I expected BFB2 to be cleared to 0 (default).

  • However, after a system reset, I observed that BFB2 is set to 1.

I would like to understand:

  1. Who sets BFB2 to 1 after an option bytes erase?

  2. Is this controlled by bootloader behavior, internal flash controller logic, or some default hardware mechanism?

This topic has been closed for replies.
TDK
TDKBest answer
May 7, 2025 1:37 PM UTC

Keil is setting those bytes. They do not change arbitrarily.

 

You can use STM32CubeProgrammer to set them if you'd like.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
May 7, 2025 12:42 PM UTC

If you want BFB2=0, perhaps set it explicitly. There is no "option byte erase" procedure at the mcu level, so this is something Keil-specific being done.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JohnFrancis
Associate III
May 7, 2025 1:05 PM UTC

In Reference Manual RM0440, the User & Read Protection Option Bytes are documented at Flash memory address 0x1FFF7800 with an ST production value of 0xFFEF F8AA. However, when I print the User & Read Protection Option Bytes, I get 0xFFFF F8AA, which does not match the documented production value.

I expected Bit 20 (BFB2) to be 0 (the default ST production value) because I had deleted the option bytes using Keil. I want to understand who sets BFB2 to 1, even though User & Read Protection Option Bytes are read-only.

I don’t necessarily want BFB2 to be 0, but initially, after deleting the option bytes, I checked and BFB2 was 0. Once the option bytes were properly set after the initial factory configuration, they were never configured again. However, now I can’t use that same logic to configure the option bytes.

TDK
TDKBest answer
May 7, 2025 1:37 PM UTC

Keil is setting those bytes. They do not change arbitrarily.

 

You can use STM32CubeProgrammer to set them if you'd like.

"If you feel a post has answered your question, please click ""Accept as Solution""."