Skip to main content
PRedd.111
Associate III
Jul 2, 2020 8:47 PM UTC
Question

Which STM32 part has the fastest ADC sampling. Is there any MCU with 1+ GSPS. Is there any way for me to use an stm32 to sample 4 inputs at 50MHz analog BW each?

I am trying to sample 4 inputs at 50MHz analog BW. Which STM32 MCU can support this? Does it have a fast interface to stream that data out?

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
Jul 2, 2020 9:06 PM UTC

Thats several orders of magnitude off the capabilities of ADC in STM32.

JW

TDK
Jul 2, 2020 10:19 PM UTC

There are dedicated, expensive ADC chips that don't meet those specs. Most you're going to get from an STM32 is on the order of 1 Msps.

"If you feel a post has answered your question, please click ""Accept as Solution""."