Skip to main content
Marco Catellani
Visitor II
June 20, 2017
Question

Which stm32 is best for making a CAN network log?

  • June 20, 2017
  • 1 reply
  • 654 views
Posted on June 20, 2017 at 10:09

I would like to build a project based on STM32 that interfaces with a CAN network. The CAN network has a 250kbps baud rate.

On this network I have to:

  • Log messages from 127 nodes with IDs between 0x381 and 0x3FF (Each node sends a message per second).
  • Send messages to nodes with id between 0x581 and 0x5FF
  • Receive response to these messages that will have IDs between 0x601 and 0x67F.

I was thinking of using an STM32 with 2 CANs. My intention is to set up 2 different filters on IDs and limit interruptions. Is that a good choice? Can it be done with only one CAN?

I have doubts about the kind and the speed of processor to use. Can an STM32F1/F0 be sufficient? Or do I need an F4?

Thanks in advance.

    This topic has been closed for replies.

    1 reply

    Jack Peacock
    Visitor II
    June 20, 2017
    Posted on June 20, 2017 at 12:39

    Whether or not to use 2 CAN interfaces depends on how you are connecting to the network.  If there's only one bus adding a second transceiver and interface won't help performance.  You are limited by the bandwidth of the bus itself, not the controller.  If it's a dual bus, something like an ISOBUS tractor or combine, then you must have 2 separate bus transceivers and interfaces.

    Unless youa re building a large number of these repeaters I'd recommend an F4, only because it gives you some margin in terms of memory buffers.  Bear in mind you may have to keep a large buffer of messages in case of heavy contention or a node failure, which can temporarily take the bus offline.

    Otherwise your application is basically a store and forward repeater, not a complex task.  Performance is limited by how much access time you can get on the bus, not the controller core.  If it's cost sensitive look at an F2. 

       Jack Peacock